779920_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

779920_en-US

779920_en-US

Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?

Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?

Re: Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?

Hi Rick,

The feedback from our product group is that there are no plans to provide something to cover the port up, unfortunately.

Best regards,

Tomas

Re: Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?

Hi Rick,

I am asking our product group to comment on this. I will update this thread as soon as I have their feedback.

Best regards,

Tomas

Re: Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?  

Hi Tomas,

Thanks for the reply.  Do you know if there are any plans in the future to provide the purchased part with a removable seal?  The reason I am asking is because it is a small SMD device and there is risk and labor at the piece part level of unpackaging, handling, applying a seal and repackaging prior to loading on the placement machine for assembly.

Thanks,

Rick. 

Re: Hi - Does the MPH6250A6T1 pressure sensor come with any options to protect (seal) the port opening during the assembly process (i.e. aqueous wash, etc.)?

Hi Rick,

No, it does not.

But yes, it is strongly recommended the port opening to be protected e.g. by adhesive Kapton tape or other means prior to the cleaning process to prevent contamination and foreign materials from being introduced into device as result of cleaning processes.  

Best regards,

Tomas

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 10:02 AM
更新者: