665952_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

665952_en-US

665952_en-US

RDMMA845X issues with Win 7 Pro.

As a retired electronics man (but total newbie with PC + dev. boards) I hope this isn't too much of a stupid question. I have bought the above board. It works great on a Win 8.1 PC, but not on the Win 7 Pro PC - which is a shame because that's the one in my hobby lab! Win 7 finds the USB device and the Demo Screen correctly identifies the chip in use, etc. But hitting any of the 'lit' buttons just generates an Exception Handler window and I can go no further than that. I don't know what Ex Handler means so am at a loss! Wisdom greatfully accepted. Tks. John

AccelerometersRe: RDMMA845X issues with Win 7 Pro.

As an addition to my original post I should say that the exception window calls this an "unhandled exception". After some internet research I updated the .net framework to the latest ver (4.6.2) in case that was the cause. But it is not! Tks. J 

标记 (1)
无评分
版本历史
最后更新:
‎02-04-2026 05:32 AM
更新人: