660929_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

660929_en-US

660929_en-US

FXTH87xx TPM sensor Pressure Measurement

I have purchased TPM sensor FXTH8705116T1- 450kpa.

I have installed it inside Tire and filled with an air pressure of 42 PSI.

The pressure value received from the sensor is 0x1FE (TPMS_COMP_PRESSURE).

From the data sheet,  0x1FE (TPMS_COMP_PRESSURE) represents pressure overflow(high). But 450kpa sensor has a range of 14 - 65 psi(100 – 450kpa).

Also when we gradually reduced the air level from tire, sensor pressure value also decreased gradually from 0x1FE (0x1EA , 0x1Ab etc.,).

For 42 psi , expected pressure value from the sensor should be around 0x122. But  receiving 0x1FE. Please help.

fxth87xx‌#fxth87xx11

Re: FXTH87xx TPM sensor Pressure Measurement

Hello Amarnath,

We need more information from you to find out what is going on.

How was the actual pressure (42PSI) measured?

Was this test performed on several samples? If not, could you do it on five or ten samples?

If the problem occurs on all samples, could you try to measure the actual pressure with another mean?

Are you sure your reference is accurate?

Best regards,

Tomas

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 09:17 AM
更新者: