648515_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

648515_en-US

648515_en-US

sensor type MPXH6300A

for sensor type MPXH6300A is there an option for a more media resistant gel ? current device has a florosilicone type gel

Pressure SensorsRe: sensor type MPXH6300A

Tomas,  In the "as received" condition there are a mix of cloudy and the clear gel on the same reel....does the cloudy appearance impact performance or is this an acceptable condition ?

pastedImage_1.png

Re: sensor type MPXH6300A

Hi Phil,

No, there is not. There are only the MPXHZ6250A and MPXHZ6400A series available with the media resistant gel.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 06:31 AM
更新者: