468682_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

468682_en-US

468682_en-US

Error FIFO FXLS8471

I'm working with a FXLS8471 sensor with SPI.
My problem is that the reading of the 32  measurements of the FIFO  does not coincide with the reading of the acceleration in the three axes. The sensor interrupted by filling the FIFO but when I try to read the 192 bytes in burst mode, the answer is incomprehensible.
Thank you

 

Carlos Canal

Intelligent Sensing FrameworkRe: Error FIFO FXLS8471

Hello Carlos,

Here some suggestions & feedbacks:

"Where axis X reading is = FF E0 (AX=0.0024g), axis Y=FD 70 (Ay=-0.0518g) and axis Z= 40 E8 (Az=0.9995g)"

Regarding your conversion, AX should be negative FFE0 (hex) = -32 signed 16 bits) = -32/2² = -4 (signed 14bits)  = -4*sensitivity (g or mg).

About your reading function, it seems good, I've got:

bool FXLS8471Q::bRead(uint8_t __u8_register, uint8_t* __au8_OutValue,uint8_t __u8_length)

{

    bool __b_result = false;

    uint8_t __u8_i;

   

    _t_cs = 0;

   

    _t_spi.write(  (__u8_register&0x7F) | (0x0<<7) ) ;

    _t_spi.write(__u8_register&0x80);

    for(__u8_i=0;__u8_i<__u8_length;__u8_i++)

    {

        __au8_OutValue[__u8_i] =  _t_spi.write(0x00) ;

    }

    _t_cs   =   1;

  

    __b_result = true;

    return __b_result;

}

but again, check your conversion...

Are you sure the FIFO is enabled? How did you configure the sensor?

Thanks,

Anthony

Re: Error FIFO FXLS8471

Hello Anthony:

I do not get properly read accelerations 32 records stored in the FIFO.

For example, a reading of the acceleration of the three axes is:   FF  E0 FD  70  40  E8

Where axis X reading is = FF E0 (AX=0.0024g), axis Y=FD 70 (Ay=-0.0518g) and axis Z= 40 E8 (Az=0.9995g)

The following data correspond to a reading of the FIFO

For example, axis X =7E  D8 , axis Y =20 60  and axis Z =00 40
7E  D8 20  60  00  40         7E  B8  20  38 00  34          7E D8  20  B8 00  30      7E D8  20  4C 00  18      7E E8  20  90 00  34         7E  F8 20  64  00 18

7E F4  20  40 00  3C          7E  F4  20  30 00  10          7E  D8  20  78  00 3C     7E C0  20  50 7F  F8      7E D0  20  40 00  44         7E  B0 20  6C  00 44

7E  E0 20  50  00 38          7E F0  20  7C 00  08           7E  E0  20  38 00  00      7E  D8 20  50  00  18      7E C0  20  5C 00  10        7E  E0 20  74  00 18

  7E E0  20  7C 00  10         7E  D8 20  90  00 10            7E  F0 20  30  00 30       7E E0  20  30  00  38      7E E8  20  60 00  44        7E  E8 20 58  00  2C

  7E  E0 20  54  00 3C         7E F4  20  88 00  58            7E D8  20  60 00  2C      7E  B8 20  6C  00 38      7E  A8 20  64  00 20         7E A8  20  64 00  44

   7E D0  20  60 00  04         7E  E0 20  58  00 7C 

La function para leer los 192 bytes es la siguiente:

void IMUREAD2(char reg1, int count, unsigned char array[]){

unsigned int i;

unsigned char value;

unsigned  char dire, dire1;

dire =reg1 &0x7F;

dire1= reg1 &0x80;

CS_FX=0;

WByteSPI1(dire);

WByteSPI1(dire1);

                for(i = 0; i < count; i++){

                               array[i]=RByteSPI1();//

                               }

Nop();

CS_FX=1;

return;

                }

Thank you very much and best regards

Carlos Canal

Re: Error FIFO FXLS8471

Hello Carlos,

Yes, the FIFO works with a 800Hz data rate. You just have to configure the CTRL_REG1 register by resetting the dr[0:2] field (to 0b000) .

I attached an application note about FIFO uses in the motion sensors if you want to take a look at.

Have a good day.

Anthony

Re: Error FIFO FXLS8471

Hello Anthony:
Thank you very much for your cooperation.
This weekend I report my code and put it on this page.
I have the following question: Can use a 800 Hz ODR to work with FIFO?
Thank you very much and best regards

Carlos Canal

Re: Error FIFO FXLS8471

Hello Carlos,

Can you share your FXLS8471 configuration?
I also would like to take a look at your drain function which empty the FIFO.

Here my configuration if you want to compare:

// CONFIG

#define FXLS8471Q_CTRL_REG1        0x2A

#define FXLS8471Q_CTRL_REG2        0x2B

#define FXLS8471Q_CTRL_REG3        0x2C

#define FXLS8471Q_CTRL_REG4        0x2D

#define FXLS8471Q_CTRL_REG5        0x2E

#define FXLS8471Q_XYZ_DATA_CFG     0x0E

// ID

#define FXLS8471Q_WHO_AM_I         0x0D

#define FXLS8471Q_WHO_AM_I_VAL     0x6A

// FIFO

#define FXLS8471Q_F_SETUP          0x09

#define FXLS8471Q_F_STATUS         0x00

bool FXLS8471Q::vInit()

{

    bool __b_result=false;

    uint8_t __u8_temp=0xFF;

    /* Check presence of the sensor to prevent SPI issues*/

    if(bRead(FXLS8471Q_WHO_AM_I,&__u8_temp,1))  

    if(__u8_temp == FXLS8471Q_WHO_AM_I_VAL)      //Check Sensor ID answer

  

    /* Confugre the sensor */

    if(bWrite(FXLS8471Q_CTRL_REG1  ,0x0))        //Standby mode

    if(bWrite(FXLS8471Q_XYZ_DATA_CFG,0x2))        //0.976mg/LSB  

  

    /* Configure the FIFO */

    if(bWrite(FXLS8471Q_F_SETUP    ,0x80))      // FIFO mode2 : stops accepting new samples when overflowed

  

    /* Configure the FIFO interrupt */

    if(bWrite(FXLS8471Q_CTRL_REG3  ,0x82))      // FIFO, interrupt active high (rising event)

    if(bWrite(FXLS8471Q_CTRL_REG4  ,0x40))      // FIFO interrupt enabled

    if(bWrite(FXLS8471Q_CTRL_REG5  ,0x40))      // FIFO interrupt pin routed to INT1

    if(bWrite(FXLS8471Q_CTRL_REG1  ,0x11))      //Set ODR to 400Hz & active mode

    {

        __b_result= true;

    }

                                      

    return __b_result;

}

#define FXLS8471Q_OUT_X_MSB         0x01

bool FXLS8471Q::bGetFIFOAccelData(int16_t __aai16_AccelData[32][3])

{

    uint8_t __au8_Buffer[192];

    int16_t __i16_SingleData;

    uint8_t __u8_i,__u8_j;

    bool __b_result;

    if(__b_result = bRead(FXLS8471Q_OUT_X_MSB,(uint8_t*)__au8_Buffer,192))

    {

        for(__u8_i=0;__u8_i<32;__u8_i++)

        {

            for(__u8_j=0;__u8_j<3;__u8_j++)

             {

            __i16_SingleData = (int16_t)( (__au8_Buffer[__u8_j*2+__u8_i*6]<<8) + __au8_Buffer[__u8_j*2+__u8_i*6+1]);

             __aai16_AccelData[__u8_i][__u8_j] =  (int16_t)( ((float)__i16_SingleData)/4.0);

            }  

        }

     

    }

    return __b_result;

}

Give me more information about your issues.

Thanks,

Anthony

Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 03:31 AM
Updated by: