384134_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

384134_en-US

384134_en-US

What is the main reason of that the MMA865x has two interrupt outputs?

MMA865x has two interrupt pins.

Are there special cases that the user should use both channel?

Or is it just for convenience?

AccelerometersRe: What is the main reason of that the MMA865x has two interrupt outputs?

Hi HJ,

One interrupt pin is typically used to indicate data-ready for processor synchronization and the second one for any of the embedded functions such as any-motion (slope) detection for wake-up, tap sensing for tap-sensitive user interface control, orientation change recognition for portrait or landscape switching, low-g/high-g detection for shock and free-fall detection, or no-motion for power saving. All these embedded interrupt functions allow for overall power savings relieving the host processor from continuously polling data.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 07:21 AM
更新者: