327509_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

327509_en-US

327509_en-US

MPX5010 vs MPX2010

Dear Freescale,

I currently use MPX2010 in a dual port configuration.  I am looking to move to the MPX5010 with the integrated amplifier but had a few questions:

1.) Is the sensor the same in the MPX2010 and the MPX5010?

2.) Are there any application recommendations for interfacing to the MPX5010?

Sincerely,

Jason

Pressure SensorsSensing PlatformsRe: MPX5010 vs MPX2010

Hi Jason Haedt,

Answering to your questions:

  1. It is a very similar sensor with the difference (that you already noticed) that the MPX5010 is on-chip amplified, but both have the same pressure range and general functionality.

  1. It is actually very simple to interface the MPX5010 since it’s already amplified, temperature compensated and calibrated, so the only think you need to add are just a few capacitors (as seen on Figure 3 of the datasheet) and the signal goes directly to your mcu’s ADC.

Click here to find all the documentation available for the MPX5010.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 06:14 AM
更新者: