322770_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

322770_en-US

322770_en-US

UART communication with KIT9Z1J638EVM Evaluation Board

I'm working on KIT9Z1J638EVM Evaluation Board. It is mentionned in the kit user guide that LIN bus can be used as SCI (UART). I need to connect  the evalboard to PC via serial cable and establish half duplex communication. Is it possible? if yes, any help of how to do that? I tried to connect the LIN bus configured as SCI to the RXD pin of RS232 cable but I can't have a correct communication.

Battery SensorsRe: UART communication with KIT9Z1J638EVM Evaluation Board

Hello Souha,

The connection is done through the SCI module of the MM9Z1_638 and the OSBDM port that will add a virtual COM port on the PC when connected. The LIN is not involved there.

This is explained in the KIT9Z1J638EVM User‘s Guide within the following note:

GPIO pins might also be connected to OSBDM to set Serial to the USB port. This is done by connecting:

TxD from SCI to one pin out of PTB[3…1], then the selected PTB to JP4-2.

RxD from SCI to one pin out of PTB[4…1], then the selected PTB to JP4-1.

Insure that the two selected PTB pins have no other setting (voltage sensing external divider, external temperature sensing setup), which might conflict with the 5.0 V digital IO setup.

So there you have to connect wires from selected PTBs to the right position on JP4.

Please refer to the KIT9Z1J638EVM User‘s Guide.

I hope it helps.


Regards,

Tomas

标记 (1)
无评分
版本历史
最后更新:
‎02-04-2026 07:15 AM
更新人: