The NXP zsdk information specifies that RW612 supports scantternet topology, which allows for a peripheral to be connected to multiple centrals nxp-zsdk/doc/wireless/release-notes/topics/bluetooth_radio_features.md at main · nxp-zephyr/nxp-zsdk....
How many connections are supported from a peripheral device to different BLE centrals?
Are there any constraints across these connections? Shall they use same PHY, connection parameters or other traits ?
Best regards Tonny Bing
You may check the datasheet for different topology.There are one antenna topology and two antenna topology using internal SPDT