Hi all,
I'm trying to bring up a Sony IMX219 camera on the FRDM-IMX95 (imx95-15x15-lpddr4x-frdm) using AN15033 (i.MX Camera Software Pack, BSP LF6.18.2-1.0.0), section 3.2 (precompiled binaries). The camera is not detected.
**What I did**
- Booted the prebuilt LF6.18.2-1.0.0 image
- Ran copy_binaries.sh from the IMX219 binaries directory (i.MX95-15x15-FRDM-LPDDR4x)
- In U-Boot: setenv fdtfile imx95-15x15-frdm-imx219-isp.dtb; saveenv; boot
- Camera: standard 15-pin IMX219 module (the module and FPC cable both are connected and pin to pin match and the camera is working with STM32mp2 and Rpi).
**What I see**
-nxp-neo-uguzzi/ and cam -l (with LIBCAMERA_IPA_MODULE_PATH=/usr/lib/libcamera/ipaLIBCAMERA_PIPELINES_MATCH_LIST='nxp/neo,imx8-isi,uvc' exported):
libcamera v0.0.0+6489-lf-6.18.2-1.0.0
Available cameras:
(empty)
dmesg:
root@imx95-15x15-lpddr4x-frdm:~# dmesg | grep "imx219"
[ 0.479570] /soc/bus@42000000/i2c@42540000/imx219@10: Fixed dependency cycle(s) with /soc/csi@4ad30000
[ 0.533110] /soc/csi@4ad30000: Fixed dependency cycle(s) with /soc/bus@42000000/i2c@42540000/imx219@10
[ 0.670857] /soc/bus@42000000/i2c@42540000/imx219@10: Fixed dependency cycle(s) with /soc/csi@4ad30000
[ 0.712509] /soc/bus@42000000/i2c@42540000/imx219@10: Fixed dependency cycle(s) with /soc/csi@4ad30000
[ 0.784500] /soc/bus@42000000/i2c@42540000/imx219@10: Fixed dependency cycle(s) with /soc/csi@4ad30000
[ 0.802395] /soc/csi@4ad30000: Fixed dependency cycle(s) with /soc/bus@42000000/i2c@42540000/imx219@10
[ 3.664050] /soc/csi@4ad30000: Fixed dependency cycle(s) with /soc/bus@42000000/i2c@42540000/imx219@10
[ 3.673513] /soc/bus@42000000/i2c@42540000/imx219@10: Fixed dependency cycle(s) with /soc/csi@4ad30000
[ 9.425624] imx219 3-0010: supply VANA not found, using dummy regulator
[ 9.436000] imx219 3-0010: supply VDIG not found, using dummy regulator
[ 9.443871] imx219 3-0010: supply VDDL not found, using dummy regulator
[ 9.462659] imx219 3-0010: Error reading reg 0x0000: -5
[ 9.468287] imx219 3-0010: error -EIO: failed to read chip id 219
[ 9.478088] imx219 3-0010: probe with driver imx219 failed with error -5
After reseating the camera the error changed to -5 (-EIO), same "failed to read chip id".
i2cdetect: nothing at 0x10 on i2c-2 (42530000.i2c) or i2c-3 (42540000.i2c). Only unrelated devices show up (UU at 0x33, 0x4c, 0x62 on bus 3; 0x50 and 0x52 on bus 2).
The imx219 module is loaded, the DT node exists, and the neoisp probe succeeds, so this looks like the sensor is not reachable/powered rather than a libcamera or driver issue.
**Observations**
- The DT node is imx219@10 under /soc/bus@42000000/i2c@42540000 (i2c-3). AN15033 section 3.4 shows the path as .../i2c@42530000/imx219@10, which doesn't match what I have. Is this a typo in the note?
- The node has reset-gpios. gpioinfo shows "MIPI-CSI camera reset" (line 19) as an output with no consumer after the probe fails.
**Questions**
1. AN15033 connects the camera via the RPI-CAM-MINISAS adaptor plus a 22-pin to 15-pin FPC cable. Is that adaptor required, or is a plain 15-to-22-pin cable enough?
Note: Pin to pin matched.
2. Has anyone gotten the IMX219 working on the FRDM-IMX95 with this software pack, and if so, with which exact module and cable?
Here is the camera im using : https://probots.co.in/8mp-imx219-camera-module-77-fov-raspberry-pi-5.html
BR
Aman Sharma