2419514_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2419514_en-US

2419514_en-US

Enable FLEXCAN for IMXRT1064

Hi, 

I am working on MIMXRT1064CVJ5B, is FLEXCAN supports on these PINs 

GPIO_AD_B1_12 : Chip Select

GPIO_AD_B1_13 : MISO

GPIO_AD_B1_14 : MOSI 

GPIO_AD_B1_15 : CLK

I have connected a NAND Flash on these Pin, Does any example code available ? 


Re: Enable FLEXCAN for IMXRT1064

Hi 

You can find the available pins for the FlexCAN modules in Table 10-1 Muxing Options, of the i.MX RT1064 Processor Reference Manual.

You can also find FlexCAN examples available for the i.MX RT1064 in the SDK. I would recommend reviewing the available examples and using the one that most closely matches your application's requirements as a reference for your implementation.

Best Regards,
Pablo

标记 (1)
无评分
版本历史
最后更新:
星期五
更新人: