Hello experts,
I configured .mex file for controller S32K342 with RTD 7.0.0.
I am getting following error:
I copied the configuration from S32K344 configuration with RTD 6.0.0 (because pin configuration and Peripherals configuration are same).
I put all the counter bus correctly which we require.
few screenshots for Emios_Mcl_Ip
Thanks.
Thank you for quick response.
No, I did not copy entirely. I created new project with choosing 342 controller and copied the peripheral configurations. Not the whole project.
Hope this helps.
Thanks.
Thank you for the project.
I copied the .mex file into one of my projects and, interestingly, I don't see any errors when generating code from it..
Could you please clarify what you mean by: "I copied the configuration from an S32K344 configuration with RTD 6.0.0"? Did you copy the .mex file from a project that was originally created with RTD 6.0.0?
Regards,
Daniel
Please the refer the configuration shared.
Thanks.
Hello @sbidkar,
Can you please share the .mex file?
Thank you
Thank you, Daniel, for your response.
I am using IDE version 3.6.4
BR.
Hi @sbidkar,
Last time, I opened the .mex file in S32 Design Studio 3.6.9 with RTD 7.0.1, and the issue did not occur. When I tested it in S32 Design Studio 3.6.5 with RTD 7.0.0, I was able to reproduce the issue.
Which IDE version are you using?
I haven't found an existing report for this issue yet. I'll check with the IDE team and get back to you.
Thank you,
BR, Daniel