2418265_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2418265_en-US

2418265_en-US

MCUXpresso IDE v24.12 [Build 148] [2025-01-10] debug attach without .AXF image download

Dear Support

I need to use the MCUXpresso debugger (JLINK) without download the .AXF image (I need to reprogram some flash sector on runtime), so I deselected the "Load image" option (see attached image). It works but is not possible to restart the program to the main 

pberna67_1-1791026048228.png


even if the related checkbox in the Debug Configuration -> Startup is selected.


pberna67_0-1791025854437.png


Is it possible to restart the program assuming that no change is done in the flash memory even if .AXF is not loaded ?

Regard

Paolo

Tags (1)
No ratings
Version history
Last update:
16 hours ago
Updated by: