This hands-on walks you through everything that happens before you ever write a line of application code: unboxing your FRDM i.MX 95 Pro board, getting acquainted with its layout and ports, powering it on, and confirming a healthy first boot from the on-board eMMC. By the time you are done, you will be comfortable using both the i.MX System Manager console and the Linux command line to confirm exactly what hardware you have in front of you.
By the end you will be able to:
You need very little to get started:
That's it — no display or camera is required for this hands-on.
Watch the full hands-on walkthrough below, then follow along on your own board.
Once the board has booted, open a terminal on the debug console and run the following commands to confirm the Linux environment and the hardware resources available to you.
# 1) Linux version
uname -a
# 2) Storage devices
lsblk
# 3) Verify CPU numbers and architecture.
lscpu
# 4) SoC Id and Family
cat /sys/devices/soc0/soc_id
cat /sys/devices/soc0/family
# 5) RAM memory available
cat /proc/meminfo | head -20
# 6) network peripherals and addresses
ip addr
# 7) List Video Encoders and Decoders
v4l2-ctl --list-devices
# GPU specs and capabilities
vulkaninfo --summary
# 9) Print available GPIOs
gpioinfo
Next, switch to the i.MX System Manager (SM) console to inspect the board at the system level — Logical Machines, boot times, power rails, and clocks.
# 1) System manager version, Board, Revision, Silicon etc
info
# 2) Logical Machines information
lm info
# 3) Boot time of each Logical machine
btime
# 4) Power status of each peripheral
power.r
# 5) Clocks status
clock.r
| Symptom | What to check |
|---|---|
| Power LED is on but there is no output on the console |
|
In this hands-on, you:
If you have not already, watch the module video above for the full walkthrough, and check out the rest of the FRDM Training Hub for the next hands-on in the series.