Welcome to IW610 M.2 and FRDM Adapter Product Training! This page provides access to training materials, presentations, demos, recordings, and supporting resources related to the IW610 M.2 development card and the FRDM adapter. While live Q&A support will be available during the training period, all content will remain accessible for future reference and self-paced learning.
Instructions
To get started with the IW610 M.2 and FRDM Adapter training, you will need to have your FRDM-MCXN947, IW610G-M2 and FRDM Adapter board in hand and perform the set-up operations according to the IW610G-M2 and FRDM-ADPT-MCX-M2 Getting Started Page which is a pre-requisite.
Step 1. Mandatory pre-work before starting with the labs:
Step 2. After completing the pre-work, download the lab guides. Each lab has its own guide document and a video guide you can use as support material in case you have any question at any step:
Description
This demo connects the IW610G-M2 to an FRDM-MCXN947 using an FRDM-M2-ADAPTER board and sends temperature measurements to an HTTPS server over Wi-Fi. Also creates an access point to enable connections. The online dashboard can also be used to wirelessly control the onboard LEDs. (End applications: home automation, industrial monitoring)
Description
This demo connects the IW610G-M2 to an FRDM-MCXN947 using an FRDM-M2-ADAPTER board and uses a camera module to stream real-time video over Wi-Fi to a laptop or another FRDM-MCXN947 with an IW610G-M2. The captured video is displayed on an LCD-PAR screen (In case to use a FRDM-MCXN947). (End application: Interphone, security camera)
Step 3. Review the support material and useful links to get you up to speed with some product information, M.2 development card and FRDM adapter information and getting started. Below also includes additional reading material.
IW610 M2 Module | NXP Semiconductors
Getting Started with IW610G-M2 | NXP Semiconductors
https://nww.preview-cloud.nxp.com/pages/:FRDM-ADPT-MCX-M2
Getting Started with FRDM-ADPT-MCX-M2 | NXP Semiconductors
Community Support
If you have questions regarding this training, please leave your comments in our Wireless Community! here