Dear all
I've downloaded sdk.sdk_2.x_lpcxpresso54114 with only FreeMASTER examples. It works correctly but I have a problem if I select the Edge support in the Option panel of FreeMASTER
in that case the Welcome Screen appears:
Clicking on Board's Built-In Welcome Page, one time, than wait 10 second or more.... nothing happen. After 10 second click again (second time) than the page appears:
without icons, and if you click on the links a strange behavior happen (a save window appears if you try, for example, to click on readme.txt link)
Vice versa ,If you select Internet Explorer in the option Option panel of FreeMASTER the result is almost right
read me link opens the internal readme.txt file but if you click on Demo Project file link
An msxbox with error appers anyway
The problem is that I need to support recent browsers using RPC-JSON script approach and your and also my attached html file don't work. Please test my .h file in your platform too. It refers to the same variables and command of the sdk firwmare
Regards
Paolo