S32K142EVB-Q100 evaluation board with S32 Design Studio 3.6.11I am having trouble using the S32K142EVB-Q100 evaluation board with S32 Design Studio 3.6.11
I used the S32DS Extensions and Updates to install S32K1xx Development Package and S32K1_S32M24X Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP07
My problem is that when I create a new project with S32K142 I cannot use the S32 Configuration Tools it says there is no data. I can't configure the pins or anything.
How can I get started with this setup?

Re: S32K142EVB-Q100 evaluation board with S32 Design Studio 3.6.11Hi,
SW32K1_S32M24x_RTD_R21-11_3.0.0_QLP07_D2606 contains only a few Driver Plugins, refer to package Release note.
First install S32K1_S32M24X Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP06 (SW32K1_S32M24x_RTD_R21-11_3.0.0_QLP06_D2603_DesignStudio_updatesite.zip), and then install S32K1_S32M24x Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP07 if needed it.
Also don't forget to select GCC v10.2 toolchain when creating new Project. If this is not installed in your S32DS add it as well through Extension&Updates.
BR, Petr