Hi NXP Team,
We are currently working with the NXP i.MX95 19×19 EVK (IMX95LPD5EVK-19) and Android Automotive OS (AAOS) 16.
Our requirement is to use a camera module that is officially supported by the i.MX95 BSP.
We previously evaluated the Sony IMX219, IMX258 and IMX477 camera modules listed in AN14853. However, we understand that the Innowave IMX258 is not officially supported in the i.MX95 BSP.
Based on the guidance from NXP, we understand that the IMX95-OS08A20 is an NXP-supported camera module for the i.MX95 19×19 EVK.
We would like to confirm the following for our specific use case:
1. Is the IMX95-OS08A20 officially supported with AAOS 16 on the i.MX95 19×19 EVK (IMX95LPD5EVK-19)?
2. Which exact NXP BSP / AAOS 16 release should be used for the IMX95-OS08A20?
3. Is the required camera driver and ISP support already included in the AAOS 16 BSP?
4. Are any additional patches, software packages or configuration changes required to enable the OS08A20?
5. Which Device Tree / DTB configuration should be used for the OS08A20 camera on the 19×19 EVK?
6. What camera resolutions and frame rates are supported with AAOS 16?
7. Is there an EVS configuration or sample application available for using the OS08A20 with AAOS 16?
8. Please confirm the exact camera module / part number and required cable or adapter that we should purchase.
9. If possible, please provide the recommended purchase information or NXP distributor information for the IMX95-OS08A20.
Our current environment is:
Board:
NXP i.MX95 19×19 EVK (IMX95LPD5EVK-19)
Software:
Android Automotive OS 16
BSP:
NXP i.MX95 BSP
We would like to proceed with purchasing the camera only after confirming its compatibility with our exact AAOS 16 + BSP environment.
NXP reference:
https://www.nxp.com/design/design-center/development-boards-and-designs/IMX95-OS08A20
Thank you.
Hello,
The OS08A20 is not a camera supported in the AAOS for the i.MX95, for this processor we support OX03C10 and the AP1302 camera sensors.
Best regards/Saludos,
Aldo.
Hi Aldo,
Thank you for the clarification.
We understand that the OS08A20 is not supported in AAOS for the i.MX95, and that the supported camera solutions for AAOS are OX03C10 and AP1302.
Our requirement is specifically for AAOS 16 on the i.MX95 19×19 EVK (IMX95LPD5EVK-19).
Could you please provide the following information for the supported camera options?
Our target environment is:
Board: NXP i.MX95 19×19 EVK (IMX95LPD5EVK-19)
Software: Android Automotive OS 16
BSP: NXP i.MX95 BSP
We would like to confirm the exact supported hardware and required accessories before proceeding with the purchase.
Thank you for your support.
Best regards,
Gnana Prasanna