2416969_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2416969_en-US

2416969_en-US

Error while installing the QCVS package in CW_PA_v10.5.1

Hi,

I need to create a QorIQ Configuration Project for PBL and therefore need to install the QCVS package.

I downloaded "QCVS Offline Installation Packages for CodeWarrior for Power Architectures Rev 4.5.zip" from the support portal some time ago. Recently, I installed CodeWarrior 10.5.1 on a new laptop.

However, I am unable to install or add the QCVS package to CodeWarrior. During the installation, I encounter the following error:

Vimalprasad_0-1790665552305.png

Please help me to resolve this issue.


Regards,

Vimalprasad.

Re: Error while installing the QCVS package in CW_PA_v10.5.1

Please uninstall CodeWarrior software on your PC.

Please download "QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5.zip" and  “CodeWarrior Development Studio for Power Architecture v10.5.1 – Windows.exe” from the following link

https://support.nxp.com/s/case/500Te00000gyh6mIAA/community-error-while-installing-the-qcvs-package-...


Please install CodeWarrior for PA 10.5.1 first. Then open CodeWarrior IDE in a new workspace and install "QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5.zip" from Help->Install New Software->Add->Archive in CodeWarrior IDE.

Re: Error while installing the QCVS package in CW_PA_v10.5.1

Hi @yipingwang ,

Thanks for your response,

I have tried in the new workspace, but still I'm getting this error while installing.

Is there any latest version of QCVS tool is there for CW_PA_v10.5.1?

Regards,

Vimalprasad.

Re: Error while installing the QCVS package in CW_PA_v10.5.1

Please open CodeWarrior IDE in a new workspace first and install QCVS 4.5 from Help->Install New Software->Add->Archive in CodeWarrior IDE.

Re: Error while installing the QCVS package in CW_PA_v10.5.1

Hi @yipingwang ,

I'm still getting this following error.

while adding this QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5.zip.

Vimalprasad_0-1791355992739.png


It shows the "path" parameter was not set in the "processcheck" action.

Regards,

Vimalprasad M

Re: Error while installing the QCVS package in CW_PA_v10.5.1

What OS are you using? Windows 11?

Re: Error while installing the QCVS package in CW_PA_v10.5.1

Hi @yipingwang ,

Thanks for your reply,

 Is there any way to install CW 10.5.1 and QCVS 4.5 on a Windows 11?

Or, is there any updated QCVS version is there for Window 11?

Re: Error while installing the QCVS package in CW_PA_v10.5.1

I also reproduced your problem on my Windows 11 OS environment.

I suggest you install CW 10.5.1 and QCVS 4.5 on a Windows 10 VM.

Re: Error while installing the QCVS package in CW_PA_v10.5.1

Hi @yipingwang ,

      Yes, I'm using Windows 11.

Re: Error while installing the QCVS package in CW_PA_v10.5.1

We don't have new version QCVS software for Windows 11 so far.

Sorry for the inconvenience. 


タグ(1)
評価なし
バージョン履歴
最終更新日:
2 週間前
更新者: