2416746_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2416746_en-US

2416746_en-US

No source available for "(gdb[23].proc[42000].threadGroup[i1],gdb[23].proc[42000].OSthread[1]).threaAfter debugging the program, the message "No source available for '(gdb[23].proc[42000].threadGroup[i1], gdb[23].proc[42000].OSthread[1]).thread[1].frame[0]' " popped up.The "RESUME" button is gray. The software I am using is S32 Design Studio for ARM Version 2018.R1. Could you please tell me how to solve this problem? Thank you. S32K144EVBRe: No source available for "(gdb[23].proc[42000].threadGroup[i1],gdb[23].proc[42000].OSthread[

Hi,

The message typically indicates that the debugger stopped in a fault handler or at an invalid address where no source code is available. Please try a clean rebuild, power-cycle the board, and restart the debug session. Also verify that the correct *.elf file is selected in the GDB PEMicro debug configuration.

Additionally, please test whether the issue can be reproduced with a standard NXP S32K144 example project. This will help determine if the problem is application-specific.

Please also check which update level of S32 Design Studio for ARM 2018.R1 you currently have installed. If you are not using Update 11 (or newer), we recommend applying the update, as it contains fixes and SDK updates for S32K1xx devices.

BR, Petr

タグ(1)
評価なし
バージョン履歴
最終更新日:
昨日
更新者: