We are developing a custom board using the PHYTEC phyCORE-i.MX8M Plus SOM and are reviewing the Ethernet pinmux for migration from the existing RGMII interface to MII. The PHYTEC SOM pin A25 is associated with the i.MX8M Plus ENET_RXC signal. In the i.MX8MP pinmux, ENET_RXC supports ALT0 = CCM_ENET_QOS_CLOCK_GENERATE_RX_CLK and ALT1 = ENET_QOS_RX_ER. We need clarification regarding the correct pin assignment and interface requirements for the intended MII configuration. Specifically, is ENET_RXC required for the MII receive interface, or can the required RX_ER function be assigned to another suitable i.MX8M Plus pad/GPIO? If a different pad can be used, please provide the recommended pin mapping. We also need confirmation of whether the i.MX8M Plus ENET_QOS controller supports the intended MII interface and whether any IOMUX, MAC, device-tree, GPR, or PHY configuration changes are required. Please advise on the recommended Ethernet pin mapping and configuration for the i.MX8M Plus with the PHYTEC phyCORE SOM.
Hi,
Thank you for your interest in NXP Semiconductor products,
i.MX 8M Plus does not support MII, please refer to the following extract from RM:
Seamless interface to commercial ethernet PHY devices via one of the following:
- a 2-bit Reduced MII (RMII) operating at 50 MHz.
- a (double data rate) 4-bit Reduced GMII (RGMII) operating at 125 MHz.
For signal mapping, you can refer to i.MX 8M Plus DS.
Regards