2415119_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2415119_en-US

2415119_en-US

Oscillator transconductance question of S32K144

Hello:

In my application design, a 8MHz crystal is used and the SCG_SOSCCFG[RANGE] is set to 2b11, therefore the gmXOSC shall be 16mA/V minimum and 47mA/V maximum

Stanley_Xu_0-1790056309153.pngStanley_Xu_0-1790056309153.png

And I followed the equation gm_crit = 4 * (ESR + RS) * (2πF)^2 * (C0 + CL)^2 to calculate and compare 5*gm_crit to the datasheet value. Should I use 16mA/V or use 47mA/V ?

I don't know if 16 ~47mA/V means part to part variation. If so, from WCCA perspective, I think I shall guarantee the 5*gm_crit < 16mA/V. However, what confused me is in the document AN5426 page 11. The given calculation example uses 47mA/V as criteria.

Stanley_Xu_1-1790056639984.pngStanley_Xu_1-1790056639984.png

Can some one help me to clarify? Thank you!


Re: Oscillator transconductance question of S32K144

Hello @Stanley_Xu,

Strictly for WCCA, use the minimum gmXOSC = 16 mA/V. The 16–47 mA/V range reflects combined process (part-to-part), voltage, and temperature variation — any given part will deliver a gmXOSC somewhere in that range. The datasheet criterion gmXOSC > 5 × gm_crit guarantees proper oscillation startup and 5x gm_crit can be considered as very safe, while 3x gm_crit is still safe.

Regarding AN5426: the example uses 47 mA/V (max) for illustration, not as a WCCA.

On the other hand, the datasheet also notes: "RS should be selected carefully to have appropriate oscillation amplitude for both protecting crystal or resonator device and satisfying proper oscillation startup condition."


Regards,

Daniel

标记 (1)
无评分
版本历史
最后更新:
星期三
更新人: