2415037_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2415037_en-US

2415037_en-US

jailhouse DTS for 9x9 imx.93

Hi - Do you provide DTS files for jailhouse on the 9x9 imx.93?  I can only find ones for the 11x11.

Thanks

David

Re: jailhouse DTS for 9x9 imx.93

Hello,

This device tree will be included in the next BSP release.

// SPDX-License-Identifier: (GPL-2.0+ OR MIT)
/*
 * Copyright 2023 NXP
 */

/dts-v1/;

#include 

/ {
	model = "NXP i.MX93 9x9 QSB";
	compatible = "fsl,imx93-9x9-qsb", "fsl,imx93";
	interrupt-parent = <&gic>;
	#address-cells = <2>;
	#size-cells = <2>;

	aliases {
		mmc0 = &usdhc1;
		serial1 = &lpuart2;
	};

	cpus {
		#address-cells = <1>;
		#size-cells = <0>;

		A55_0: cpu@0 {
			device_type = "cpu";
			compatible = "arm,cortex-a55";
			reg = <0x0>;
			enable-method = "psci";
			#cooling-cells = <2>;
		};
	};

	psci {
		compatible = "arm,psci-1.0";
		method = "smc";
	};

	gic: interrupt-controller@48000000 {
		compatible = "arm,gic-v3";
		reg = <0 0x48000000 0 0x10000>,
		      <0 0x48040000 0 0xc0000>;
		#interrupt-cells = <3>;
		interrupt-controller;
		interrupts = ;
		interrupt-parent = <&gic>;
	};

	timer {
		compatible = "arm,armv8-timer";
		interrupts = ,
			     ,
			     ,
			     ;
		clock-frequency = <24000000>;
	};

	clk_dummy: clock-dummy {
		compatible = "fixed-clock";
		#clock-cells = <0>;
		clock-frequency = <0>;
		clock-output-names = "clk_dummy";
	};

	clk_400m: clock-400m {
		compatible = "fixed-clock";
		#clock-cells = <0>;
		clock-frequency = <200000000>;
		clock-output-names = "200m";
	};

	osc_24m: clock-osc-24m {
		compatible = "fixed-clock";
		#clock-cells = <0>;
		clock-frequency = <24000000>;
		clock-output-names = "osc_24m";
	};

	pci@fd700000 {
		compatible = "pci-host-ecam-generic";
		device_type = "pci";
		bus-range = <0 0>;
		#address-cells = <3>;
		#size-cells = <2>;
		#interrupt-cells = <1>;
		interrupt-map-mask = <0 0 0 7>;
		interrupt-map = <0 0 0 1 &gic GIC_SPI 227 IRQ_TYPE_EDGE_RISING>,
				<0 0 0 2 &gic GIC_SPI 228 IRQ_TYPE_EDGE_RISING>,
				<0 0 0 3 &gic GIC_SPI 229 IRQ_TYPE_EDGE_RISING>,
				<0 0 0 4 &gic GIC_SPI 230 IRQ_TYPE_EDGE_RISING>;
		reg = <0x0 0xfd700000 0x0 0x100000>;
		ranges = <0x02000000 0x00 0x10000000 0x0 0x10000000 0x00 0x10000>;
	};

	soc@0 {
		compatible = "simple-bus";
		#address-cells = <1>;
		#size-cells = <1>;
		ranges = <0x0 0x0 0x0 0x80000000>,
			 <0x28000000 0x0 0x28000000 0x10000000>;

		aips1: bus@44000000 {
			compatible = "fsl,aips-bus", "simple-bus";
			reg = <0x44000000 0x800000>;
			#address-cells = <1>;
			#size-cells = <1>;
			ranges;

			lpuart2: serial@44390000 {
				compatible = "fsl,imx93-lpuart", "fsl,imx8ulp-lpuart", "fsl,imx7ulp-lpuart";
				reg = <0x44390000 0x1000>;
				interrupts = ;
				status = "disabled";
			};
                };

		aips3: bus@42800000 {
			compatible = "fsl,aips-bus", "simple-bus";
			reg = <0x42800000 0x800000>;
			#address-cells = <1>;
			#size-cells = <1>;
			ranges;

			usdhc1: mmc@42850000 {
				compatible = "fsl,imx93-usdhc", "fsl,imx8mm-usdhc";
				reg = <0x42850000 0x10000>;
				interrupts = ;
				fsl,tuning-start-tap = <20>;
				fsl,tuning-step= <2>;
				status = "disabled";
			};
                };
	};
};

&lpuart2 {
	clocks = <&osc_24m>;
	clock-names = "ipg";
	status = "okay";
};

&usdhc1 {
	clocks = <&clk_dummy>,
		 <&clk_dummy>,
		 <&clk_400m>;
	clock-names = "ipg", "ahb", "per";
	bus-width = <8>;
	non-removable;
	status = "okay";
};

Best regards.

Re: jailhouse DTS for 9x9 imx.93do you also have the matching root cell config file for qsb jailhouse on the 9x9?
thanks
タグ(1)
評価なし
バージョン履歴
最終更新日:
木曜日
更新者: