manager:
We are currently using your FS32K144UAT0VLLT, 112MHz, LQFP-100, with an operating temperature range of -40°C to 105°C.
The design is for a gasoline engine ECU for automobiles, and the goal is to replace it with an automotive-grade one. The current selection is FS32K144HAT0MLLT, LQFP-100, 80MHZ, LQFP100, with an operating temperature of -40°C to 125°C.
Excuse me:
1. Can the two microcontrollers be interchanged pin-to-pin? Only their clock speeds and operating temperatures differ?
2. Are there any microcontrollers that can be pin-to-pin replaced with the FS32K144UAT0VLLT, with a main frequency of 112kHz and automotive grade? Please send the model number, thank you!
3. In FS32K144HAT0MLLT, does A represent CAN FD, FlexIO, or Security? What is the difference between FS32K144HFT0MLLR, where F represents CAN FD and FlexIO? What do CAN FD, FlexIO, and Security mean?
4. We purchase from websites like Taobao, but we're concerned about the legitimacy of these channels. Could you please send us a link to the NXP microcontroller distributor in North China or their contact information? Thank you!
Hi@ YF666666
Senlent_0-1789959640629.png
1. Can the two microcontrollers be interchanged pin-to-pin? Only their clock speeds and operating temperatures differ?
Yes
2. Are there any microcontrollers that can be pin-to-pin replaced with the FS32K144UAT0VLLT, with a main frequency of 112kHz and automotive grade? Please send the model number, thank you!
Pin-to-pin connectors can only be from the same series. For example, some models of S32K144 or S32K146 have the same pins and package.
You can find it in the attachment based on the ordering information above.
3. In FS32K144HAT0MLLT, does A represent CAN FD, FlexIO, or Security? What is the difference between FS32K144HFT0MLLR, where F represents CAN FD and FlexIO? What do CAN FD, FlexIO, and Security mean?
Yes, there is no difference, except that F does not support Security, meaning this chip does not support the CSE module.
It supports CAN FD, FLEXIO module, and Security (CSEc engine).
4. Information about Distributors:
You can find information on all our distributor partners in China at the link below. You can choose any distributor:
https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS#CHINA