2414645_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2414645_en-US

2414645_en-US

USB implementation on m7 core for i.MX 8M Nano processor

I need some guideance for implementing usb for i.MX 8M Nano processor m7 core, I used the nxp sdk for it. But the drive is not responding back and the signal from the controller is weak.

Re: USB implementation on m7 core for i.MX 8M Nano processor

Hello,

Unfortunately, there is no driver available for USB in the official i.MX SDK release.

It may be possible to port it from other devices for example i.MXRT, but the PHY and USB non-core registers are different, and it will not be straightforward to port but, needs to be implemented in your side.

Best regards.

Tags (1)
No ratings
Version history
Last update:
‎09-19-2026 03:40 AM
Updated by: