2413420_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2413420_en-US

2413420_en-US

EL2 Monitor: Simplifying Software Partitioning for Automotive Safety Systems

The automotive industry is undergoing a fundamental architectural shift. Where vehicles once relied on dozens of dedicated ECUs — one function, one controller — modern designs are consolidating multiple software functions onto a single, powerful processor. This consolidation reduces cost, weight, and complexity, but it introduces a critical challenge: how do you run a safety-critical AUTOSAR brake control application on the same chip as a less-critical body control stack, and guarantee they can never interfere with each other?

Full hypervisors are one answer — but they come with significant drawbacks. They are complex to integrate, expensive to license, difficult to certify to ISO 26262, and introduce latency that real-time systems cannot tolerate. NXP's EL2 Monitor (EL2M) was designed to solve exactly this problem: delivering robust, hardware-enforced software isolation with the simplicity, determinism, and safety pedigree that automotive programs demand.


What Is EL2 Monitor?


EL2 Monitor is a partitioning hypervisor that runs at Exception Level 2 (EL2) — the hypervisor privilege level defined by the Arm® architecture — on Arm® Cortex®-R52 cores. It sits between the hardware and the application software, acting as a lightweight isolation layer that enforces strict boundaries between software partitions running on the same processor.

In simple terms: EL2 Monitor takes a single physical processor and divides it into independent, isolated software environments — called R52 partitions — each running its own RTOS instance with exclusive access to its assigned resources. A fault, crash, or security breach in one partition cannot affect any other.

Unlike a full hypervisor, EL2 Monitor does not perform CPU scheduling, device virtualization, or dynamic resource management. Its scope is deliberately narrow: isolate partitions, protect shared hardware resources, and do so in a way that is statically configured, deterministic, and certifiable to ASIL D. This focused design philosophy is what makes it practical for production automotive programs.


The Core Problem: The Shared GIC Distributor


To understand why EL2 Monitor exists, it helps to understand a specific hardware constraint of the Arm Cortex-R52 architecture. In an R52-based Real-Time Unit (RTU), every two or four cores share a single GIC (Generic Interrupt Controller) Distributor — the hardware block that routes interrupts to cores. Without protection, any software running on one core has direct access to the GIC Distributor and could — accidentally or maliciously — reroute or disable interrupts belonging to another core's partition. This makes true isolation impossible without a dedicated software layer at EL2.


EL2 Monitor fills this gap. It intercepts all GIC Distributor accesses from partitions and virtualizes them, giving each partition its own exclusive Virtual GIC Distributor while the real hardware GIC remains protected.


nxf94150_1-1789390949734.png

How It Works: Two Virtualization Modes

 

Trap & Emulate


GIC Distributor accesses from EL1 software are automatically trapped to EL2, where EL2 Monitor validates and emulates them. The EL1 application is completely unaware of the virtualization — it behaves as if it has exclusive hardware access. Access operations complete in < 3 µs, making this mode suitable for standard AUTOSAR applications that require zero code changes.

 

Paravirtualization


For performance-sensitive applications, EL2 Monitor provides ready-to-use Arm CMSIS GIC Driver APIs. The EL1 software calls these APIs directly instead of accessing GIC hardware registers. This cooperative approach achieves < 1.5 µs latency — half that of full emulation — while also reducing memory usage and development time.


nxf94150_2-1789391007259.png

Hardware-Enforced Memory Protection


Beyond GIC virtualization, EL2 Monitor uses the EL2 Memory Protection Unit (MPU) to enforce strict memory boundaries between partitions in hardware. Each partition is assigned its own memory regions at configuration time. Even if an EL1 guest OS is compromised, it cannot access memory belonging to another partition.

This is complemented by NXP's XRDC (Extended Resource Domain Controller) silicon feature, creating a layered hardware + software protection architecture that is unique to NXP's S32 platform.


MRU Channel Isolation


EL2 Monitor also virtualizes MRU (Messaging Resource Unit) channels within each R52 partition. Each software entity running at a lower privilege level accesses the MRU through its own dedicated virtualized instance — inter-core communication channels cannot be accessed or corrupted by other software entities. MRU handlers are serviced in < 1.5 µs.


Static, Deterministic Configuration


All partition assignments — CPU cores, memory regions, peripherals, interrupt routing — are defined at build time using the EB Tresos or S32CT configuration plugins. There is no runtime reconfiguration, no dynamic scheduling, and no hidden shared state. This static model makes system behavior fully predictable, simplifies safety analysis, and keeps the trusted computing base small and auditable.


Safety and Quality


EL2 Monitor is qualified to ASIL D per ISO 26262:2018 — the highest automotive functional safety integrity level. Development follows NXP's Software Development Process, which is Automotive SPICE 3.1 · IATF 16949:2016 · ISO 26262:2018 · ISO 21434:2021 · ISO 9001:2015 compliant.

The complete package delivered to customers includes:

  • Quality Package: SW Traceability Matrix (Req → Design → Code → Tests), Test Specs & Reports at all levels, MISRA/CERT-C/CWE Static Analysis, Code Coverage, Benchmark & Memory Reports
  • Safety Package: Safety Manual, FMEA
  • Software Package: Source code, Release Notes, User Manual, SBOM

Development teams do not need to perform their own safety analysis of the partitioning layer — NXP provides the complete collateral, significantly reducing the certification effort for the overall system.


Developer Experience: Fits Into Your Existing Workflow


  • EB Tresos and S32CT plugins for AUTOSAR-based configuration
  • S32 Design Studio (S32DS) for build, debug, and deployment
  • Multi-compiler support for toolchain flexibility
  • Sample application included to accelerate first-time integration
  • Available via the NXP software distribution portal (Flexera)
  • 6 on-demand training videos on nxp.com: Hello World, Configuration & Build, RTOS Integration, Download & Install, Tools & Compilers, Support Channels

Supported Platforms


nxf94150_3-1789392707431.png


Why EL2 Monitor — and Why Now?


The industry trend toward software-defined vehicles and centralized compute is accelerating. Zonal and domain controllers are replacing distributed ECU networks, and the software running on these controllers is growing in both complexity and safety criticality. The need for a reliable, certified, and cost-effective partitioning solution has never been more urgent.

  • ASIL D certified — highest automotive safety integrity level, full collateral included
  • Simpler than a full hypervisor — static, deterministic, minimal trusted computing base
  • Unique NXP HW+SW stack — XRDC hardware isolation + EL2 Monitor software protection
  • Sub-1.5 µs performance — paravirtualized GIC access
  • Production-ready — full safety collateral, AUTOSAR toolchain integration, multi-platform

Explore EL2 Monitor and discover how NXP's partitioning software can help you consolidate your automotive software architecture — safely, simply, and at no additional cost.

Learn more about EL2 Monitor on nxp.com »

Daniel Hermenczi

Product Owner, EL2 Monitor — System Services, Automotive & Edge Solutions, NXP Semiconductors

Daniel is a software project manager and product owner for EL2 Monitor and IPCF at NXP Semiconductors, driving roadmap execution and customer deliveries for automotive partitioning and inter-platform communication software. He is based in Sibiu, Romania.


As vehicles consolidate more software onto fewer chips, keeping safety-critical functions truly isolated is no longer optional. EL2 Monitor delivers hardware-enforced partitioning for Arm® Cortex®-R52 — without the complexity of a full hypervisor.

タグ(1)
評価なし
バージョン履歴
最終更新日:
4 週間前
更新者: