After installing S32DS3.6.6, via install...I installed SW32K1_S32DS_Development_Pack_3.6.6_RFP_D2602.zip and SW32K1_S32M24x_RTD_R21-11_3.0.0_QLP07_D2606_DesignStudio_updatesite.zip using the New Software method. Both packages are shown as successfully installed in the Extensions list. However, I can't find K144 in the examples or by creating a new project; only K3 is available. How can I fix this?
Ex.jpgEx.jpg
exam.jpgexam.jpg
Hello @ZDDL ,
The QLP07 update site is only a patch/extension for S32K1/S32M24x RTD 3.0.0; it is not a complete RTD installation.
Please first install the base SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip package and then install QLP07 on top of it. After restarting S32 Design Studio, the S32K144 device and the corresponding examples should become available.
Best regards,
Pavel