2412281_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2412281_en-US

2412281_en-US

The CSEC and Flash driver in an S32K144 project created with S32DS3.5 cannot coexist.

I need to modify an existing S32DS3.5 project to meet the requirements of a new client. Since a Flash driver already exists, I need to add a CSEC driver. When configuring peripherals in the MEX file, I found that adding CSEC results in an error, while deleting CSEC or the Flash driver resolves the issue. How can I resolve this problem?

IDE: S32DS3.5

SDK: S32 SDK RTM 4.0.1

err.jpgerr.jpgerr.jpg

Re: S32DS3.5创建的S32K144工程CSEC和Flash驱动不能同时存在

Hello @ZDDL,

According to the SDK release notes, it is compatible with S32 Design Studio (S32DS) 3.4. Compatibility with S32DS 3.5 has not been validated, so we cannot guarantee correct functionality.

I also strongly recommend installing only one SDK or RTD version within a single IDE installation. If multiple SDK/RTD versions are required, use separate IDE installations for each version.

danielmartynek_0-1788953256888.pngdanielmartynek_0-1788953256888.pngdanielmartynek_0-1788953256888.png

BR, Daniel 

Tags (1)
No ratings
Version history
Last update:
Thursday
Updated by: