2411872_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2411872_en-US

2411872_en-US

i.MX95 PCIe connection with FPGA

This article describes a Full-Bridge PCIe reference design that connects an NXP i.MX95 SoC (acting as PCIe Root Complex) to a Lattice CertusPro-NX / Certus-NX FPGA endpoint, together with a Linux kernel driver. Updating the FPGA bitstream over PCIe is demonstrated as the reference use case, built on top of a general-purpose PCIe data-transfer, register-access and MSI-completion interface.

Hardware

  • Host / Root Complex: NXP i.MX95 SoC running Linux (DesignWare PCIe controller)
  • FPGA target / endpoint: Lattice CertusPro-NX PCIe Bridge board (Device ID 0x9C25) or Certus-NX (Device ID 0x9C1D) — Lattice Vendor ID 0x1204
  • PCIe link: 1-lane (x1), single BAR (BAR1) design
  • Interrupt: 1 MSI vector, EP→Host completion signalling
 
Board ConnectionBoard ConnectionBoard Connection

Architecture

The host application talks to the FPGA through the  kernel driver. The driver exposes BAR1 as a character device and manages two host-side DMA-coherent buffers. Because the design is a full bridge, both sides can initiate PCIe transactions: the host issues MWr/MRd to BAR1, and the FPGA (as bus master) issues its own MWr/MRd back into host memory.

Driver ArchitectureDriver ArchitectureDriver Architecture
Block Role
Application (userspace) Issues IOCTLs; supplies payload and DMA target addresses
Driver lattice_nxp_pcie_ep.c BAR1 MMIO window, SRC/DST DMA buffers, MSI completion, char device /dev/lattice_nxp_pcie_bar1
FPGA (CertusPro-NX / Certus-NX) PCIe endpoint; executes command, performs MRd/MWr, raises MSI on completion
Host memory DMA-coherent SRC and DST buffers

 

What the driver covers

The kernel module is a general-purpose PCIe endpoint transport, not a bitstream-specific driver. It contains no bitstream or image parsing — bitstream update is simply the reference application layered on top of these primitives. It provides three planes:

  1. FPGA→Host DMA path (EP-initiated bulk transfer): two host DMA-coherent buffers (SRC/DST, default 4 KB, tunable up to 1 MB). The host fills SRC, programs the FPGA SRC/DST mailbox registers and rings a doorbell; the FPGA (bus master) then moves data via its own MRd/MWr and writes results into the host DST buffer. Usable for any payload.
  2. Host↔FPGA BAR1 MMIO window: the char-device read()/write() path exposes the whole BAR1 aperture as an 8-byte-granular, byte-addressable window (readq/writeq, or paired readl/writel on 32-bit) for register/RAM access and MWr+MRd readback tests.
  3. Control + completion plane: arbitrary 32-bit BAR1 register read/write by offset (the "command" and "doorbell" registers are conventions the application chooses), plus MSI-based completion notification (atomic counter + wait/poll IOCTLs).

In short, it is a generic data-transfer + register-access + interrupt-notification interface. Bitstream loading is one application built on it; any host↔FPGA bulk transfer or register-control workflow uses the same primitives.


Driver overview — 

Probe & init: enable the PCIe device and set bus master → configure the DMA mask (32-bit default, 64-bit fallback) → map BAR1 MMIO → allocate SRC + DST coherent DMA buffers → allocate 1 MSI vector → register /dev/lattice_nxp_pcie_bar1.

IOCTL interface (9 commands):

Command Di r  Description
IOCTL_GET_INFO R Return BAR1 size, SRC/DST DMA handles, MSI IRQ number
IOCTL_FILL_SRC W Copy userspace buffer into the SRC DMA buffer
IOCTL_CLEAR_DMA – Zero the DST DMA buffer before a transfer
IOCTL_READ_DMA R Read back bytes from the DST DMA buffer after the FPGA copy
IOCTL_WAIT_MSI W Block until the next MSI fires (with timeout_ms)
IOCTL_WAIT_MSI_SINCE W Block until msi_count exceeds a given baseline (race-free)
IOCTL_GET_MSI_COUNT R Read the current MSI interrupt counter (atomic u64)
IOCTL_WRITE_REG W Write one 32-bit MMIO register in BAR1 by offset
IOCTL_READ_REG R Read one 32-bit MMIO register from BAR1 by offset

 

Driver internals

  • BAR1 read/write paths: pcie_read() / pcie_write() expose BAR1 as a char device. Accesses must be 8-byte aligned; 64-bit uses readq/writeq, 32-bit uses paired readl/writel.
  • MSI ISR: pcie_isr() atomically increments msi_count and wakes the wait-queue, unblocking WAIT_MSI / WAIT_MSI_SINCE callers. Verbosity level 2 logs each interrupt with its running count.
  • iATU resync workaround (FORCE_SYNC_IATU on probe, the driver clears and then restores the root-port Memory Base/Limit registers to force the DesignWare PCIe block to rebuild its inbound iATU translation table. This is required after an FPGA reconfiguration + PCIe remove + rescan cycle. The macro can be commented out if the workaround is not needed. Note that this alters the upstream port and can affect other PCIe devices on the same bus.

Vendor ID: 0x1204  |  Device IDs: 0x9C25 (CertusPro-NX), 0x9C1D (Certus-NX).

Module parameters

Parameter Type / default / perm Description
verbose int / 1 / 0644 0 = minimal (critical errors only); 1 = info (probe steps, DMA sizes, MSI events); 2 = chatty (all IOCTL calls, read/write rejections, MSI interrupts)
dma_bits int / 32 / 0644 DMA address width for coherent-buffer allocation. 32 = default (most platforms); 64 = use if probe fails with -ENOMEM (-12) on a 32-bit mask
dma_buf_bytes uint / 4096 / 0644 Size (bytes) of each DMA coherent buffer (SRC and DST). Min 256, default 4096

All three parameters are adjustable at load time; verbose and dma_bits can also be changed at runtime via sysfs.

 

Known limitations — unsupported PCIe transaction types

  • Configuration Read (CfgRd0 / CfgRd1) — PCIe TLP Type 0/1 config reads are not supported
  • Configuration Write (CfgWr0 / CfgWr1) — PCIe TLP Type 0/1 config writes are not supported
  • Legacy I/O Read (IORd) — x86-style I/O reads are not supported; no I/O BARs are mapped
  • Legacy I/O Write (IOWr) — x86-style I/O writes are not supported; all access goes through BAR1 MMIO

Supported: Memory Read (MRd), Memory Write (MWr), and MSI interrupt signalling via the BAR1 mailbox.

Reference

  • lattice_nxp_pcie_ep.c — Linux kernel PCIe EP driver
IMX95EVK
タグ(1)
評価なし
バージョン履歴
最終更新日:
1ヶ月前
更新者: