Looking for guidance on how to achieve the lowest possible SUSPEND mode power consumption on the FRDM-IMX95 board? With bare-metal m7 code, a55s off, I've been able to get down to ~2.2W. This is after full expander/PHY/PD_NETC power-down. How low can the FRDM-IMX95 go?
Updating my own post with my latest findings... I was able to turn off EXT_5V0 and EXT_3V3_PWR_EN and didn't see any additional improvement. I then tested DDR-self-refresh, and was able to get down to ~193mA/1.1W. I'm really wanting to go lower if possible...
You can refer to and follow our i.MX 95 Power Consumption Measurement, there are many low power use cases you can refer to.
You can close this. I was able to reliably test all the low power modes, and get to what I needed.