_0-1788779685864.png
_1-1788779725853.png
After performing a UDS‑based bootloader flash update using INCA as the host PC, a flash failure occurred on one occasion. The memory range 0x440020‑0x440027 shows '?? '. What are the possible root causes?
How to fix this issue?
如何避免这种问题的发生?
有哪些常见的原因会导致这种问题?
如何进行软件刷回操作?
Hi @代码织梦师,
I understand that the application is located at 0x440000.
However, where is the bootloader located? Is it in the same flash block?
If so, could you use a different flash block or place the flash driver in SRAM to avoid RWW issues?
At address 0x440020, there is an uncorrectable ECC error. This can occur if the flash sector was not properly erased before programming.
Therefore, please ensure that the sector is erased before programming and that any potential RWW issues are avoided.
Regards,
Daniel