gtk_window_present(window);The evidence (see attached file) strongly suggests that the startup delay is not caused by GTK application code.
The delay appears correlated with a blocking Vivante /dev/galcore ioctl within the GL rendering path. Software rendering (GSK_RENDERER=cairo) avoids the issue.
We are looking for guidance on known issues, debugging methods, configuration changes, or fixes for GTK4/OpenGL startup latency on i.MX8MP with the Vivante GPU stack.
Hi @jim777
Thank you for sharing such detailed information. Could you provide a minimal, reproducible GTK4 source code example? I need to conduct further testing in the NXP BSP.
Best Regards,
Zhiming
Hi Zhiming,
Thanks for your quick response!
Attached is a small skeleton but complete source file to test.
and the environment variables set before running:
#!/bin/sh
export XDG_RUNTIME_DIR=/run/user/0
export WAYLAND_DISPLAY=wayland-1
export GDK_BACKEND=wayland
export GSK_RENDERER=glthe relevant from weston.ini:
root@nitrogen8mp:~# cat /etc/xdg/weston/weston.ini
[core]
#gbm-format=argb8888
use-g2d=true
repaint-window=16
idle-time=0
xwayland=true
#enable-overlay-view=1
[shell]
panel-position=none
[libinput]
touchscreen_calibrator=true
#[output]
#name=HDMI-A-1
#mode=1920x1080@60
#transform=rotate-90
#[output]
#name=HDMI-A-2
#mode=off
# WIDTHxHEIGHT Resolution size width and height in pixels
# off Disables the output
# preferred Uses the preferred mode
# current Uses the current crt controller mode
#transform=rotate-90
[screen-share]
command=/usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize
#start-on-startup=true
[input-method]
path=/usr/libexec/ibus-wayland
the running time for the gtk_window_present on a desktop w/o GPU support takes some hundreds msec (< 1sec); and on the i.mx8mp device takes 9970 ms :
root@nitrogen8mp:~# gtk4-test
A: activate: before _present: 47333 ms
B: activate: after _present: 57303 ms, takes: 9970 ms
C: activate: after idele_add: 57303 ms
D: startup_task_cb: 57315 ms
^C
root@nitrogen8mp:~#
I have tried render: ngl, which leads to smear image/widgetrs/video, and Vulkan leads to critical errors: Loader Message: vkCreateDevice: Failed to validate extensions in list; Failed to realize renderer of type ‘GskVulkanRenderer’ for surface ‘GdkWaylandToplevel’: Could not find a Vulkan device with the required features.
Since out app need GPU support, and the recommended renderer under wayland/weston is still gl (UG10159 11.3.2.1 GL renderer) , I hope you can help to find a solution.
Best regards,
Hi @Zhiming_Liu
Besides what shared already, is there anything I can help to resolve the issue?
If there is any way to make it work - significantly reduce the startup time, such as configuration changes, env variable settings, different versions, or fixes/patches to the GPU driver, please let me know.
Thanks,
Hi @jim777
The GPU team is checking this issue, this will take a little while. I'll let you know as soon as there's an update.
Best Regards,
Zhiming