2411349_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2411349_en-US

2411349_en-US

MIMXRT1176DVMAB : ENET_1G RGMII operating voltages.

I would like to know that if there is the performance degradation when operating  ENET_1G  in RGMII mode with 3.3V.

Let me know if there is a specific reason to use ethernet PHY connected to ENET_1G at 1.8V.

Refer to section 6.9 Power and Ground of  RTL8211FDI-CG, the Ethernet PHY used to capable to run at 3.3/2.5/1.8/1.5V.

Re: MIMXRT1176DVMAB : ENET_1G RGMII operating voltages.

Hi,

It is okay to use i.MX RT1170 ENET 1G RGMII with 1.8V or 3.3V.

In AN14251 – i.MX RT1xxx – Ethernet Capabilities and PHY Connection, at Table 25. i.MX RT117x – ENET1G RGMII pads, you can find the MCU pins available for RGMII.

Regarding the PHY, please follow the recommendations from the vendor.

Best Regards,

Pablo

标记 (1)
无评分
版本历史
最后更新:
2 周之前
更新人: