Hi Team ,
I downloaded SAFERTOS from SAFERTOS® Archives - High Integrity Systems
I am following below S32 design studio and RTD version for SAFERTOS.(Version as they mentioned in document)
ComponentVersion
S32 Design Studio IDE | v3.6.4 |
ARM GCC Compiler | 11.4 |
S32K3 Real-Time Drivers (RTD) | 6.0.0 |
I am facing some error,
Vardhman_0-1788413006999.pngVardhman_0-1788413006999.png
I tried with different S32 design studio( Version 3.5) and RTD version RTD (2.0.0. and 5.0.0)
Is this .mex created with different version ?
Can you please provide what could be the solution.
Thanks.
Hello @Vardhman ,
The standard Variables and Expressions views normally display values only when the target is halted. Since the project uses the PEmicro debugger, please open:
Window → Show View → Other… → PE Microcomputer Systems → Real Time Expressions
Add ulTickHookCallCount to this view and resume the application. This view is specifically intended for monitoring variables while the target is running.
If required, declare the debug variable as volatile and use a debug build with low or disabled compiler optimization.
Please also refer to the following NXP Community threads, which describe how to enable and use the Real Time Expressions view for monitoring variables while the target is running:
How to watch variables live - NXP Community
Solved: How do I enable Live View for variables when debugging? - NXP Community
Best regrads,
Pavel
Hello Team,
Vardhman_0-1788508409179.pngVardhman_0-1788508409179.png
S32 was removing this double quotes and modifying path when I copied to local directory. when I corrected path. Demo RTOS is running on board.
Query - I am not able to see global variable live on S32 design studio.What setting I need to do ?? Everytime I suppose to halt the code then I can able to see variable values.
Vardhman_1-1788508801698.pngVardhman_1-1788508801698.png
Hello,
Step 1 - I installed S32-3.6.4 version RTD 6.0.0. I was facing this issue now its resolved. I was installing wrong RTD package. Now its working.
Vardhman_0-1788436426474.pngVardhman_0-1788436426474.png
Step 2 - Now I have imported the Demo SAFERTOS project provided by highintegrity systems see below snip.
Vardhman_1-1788436679719.pngVardhman_1-1788436679719.png
Step 3 - I went in manage SDK there I found that PlatformSDK_S32K344_M7 giving error or its not supported, what could be the possibility? to resolve this
Vardhman_2-1788436993601.pngVardhman_2-1788436993601.png
Step 4 - When I am creating new project not able to see SDK there still. How to resolve this ?
Step 5 - I have one query I installed 3.6.4 S32 design studio when I am installing this RTD package(6.0.0) I can see S32 design studio updated to 3.6.10. If this S32 design studio updating to 3.6.10 then this version will not supported by highintegrity systems as they mentioned compatible version for DEMO SAFERTOS IS 3.6.4 - pls give openion on this.
Step 6 - S32 design studio updated to 3.6.10
Vardhman_4-1788437960107.pngVardhman_4-1788437960107.png
Step 7 - I am getting this error after building code,
Vardhman_3-1788437895528.pngVardhman_3-1788437895528.png
I have attached RTD that i have installed.
SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite
Thanks ,
Hello @Vardhman ,
Please check that NXP GCC 10.2 is installed. Also, make sure that the GCC 10.2 toolchain is selected when creating the application project.
A similar issue is described in the following Community thread, including screenshots. Although the thread refers to the S32K1xx RTD, the reported dependency-related symptoms are similar:
S32DS 3.6.7: S32K1xx RTD 3.0.0 not detected when creating a new project
Best regards,
Pavel
Thanks this is working.