2410720_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2410720_en-US

2410720_en-US

S32K312 Firmware-Compatibility

Hello NXP Support,

We are developing TPMS controllers using S32K312HVS MCUs.
Currently sourced from China (Rev: 0P09C), we are transitioning to Malaysia production (same MCU model).

For Phase 1 validation, please confirm the following:

1. SILICON & FIRMWARE COMPATIBILITY
- Will identical firmware binary (we developed ourselves) run identically on Malaysia-sourced S32K312HVS without recompilation?
- Are there ANY silicon-level differences between China and Malaysia MCUs (same part number)?

2. SPECIFICATION CONSISTENCY
– exact match on Malaysia MCUs?
- Reset module (RGM: FREC/FRET/DREC/DRET counters) – identical behavior?
- FlexCAN peripheral (500 kbps, ISO-TP) – no variations?
- Clock accuracy & PLL lock time – same specs?

3. ERRATA & WORKAROUNDS
- Current firmware includes workarounds (RGM escalation, CAN timeout handling).
- Are these workarounds still valid on Malaysia MCUs, or do we need adjustments?
- Any NEW errata specific to Malaysia production?

4. PROCESS VARIATIONS
- Any electrical parameter shifts (timing, power, temperature coefficient)?
- ECC reliability differences on Malaysia-sourced Flash/NVM?

Please confirm: Can we use the SAME firmware binary and expect IDENTICAL product
behavior on Malaysia MCUs, or are adjustments required?

Timeline: Phase 1 validation starts in the end of September. Your quick response would be appreciated.

Re: S32K312 Firmware-Compatibility

Hello,

The S32K3xx ordering part number system uses a "N" prefix to designate "Non-China manufacturing qualified ordering part number." This is purely a sourcing/ordering designation. Critically, it does not indicate a new mask set or silicon revision — the same die/mask (0P09C) is used. The Malaysia assembly/test site is ATKL (Petaling Jaya, Malaysia), which is NXP's qualified assembly and test facility for the S32K family.

What you have to pay attention is the mask revision

petervlna_0-1788419667576.pngpetervlna_0-1788419667576.pngpetervlna_0-1788419667576.png

petervlna_1-1788419699369.pngpetervlna_1-1788419699369.pngpetervlna_1-1788419699369.png

The "N" prefix is essentially a supply chain resilience and geopolitical risk mitigation tool. It gives customers:

Guaranteed non-China assembly & test — the device is assembled and tested exclusively at non-China sites (e.g., ATKL Petaling Jaya, Malaysia). Customers who have contractual, regulatory, or policy requirements to avoid China-origin manufacturing can source the "N" variant to satisfy those requirements.

Export control / trade compliance — some customers (especially in defense-adjacent, government, or regulated automotive supply chains) are required to document and control country-of-origin for components. The "N" variant provides a clean audit trail.

Supply diversification — having both "S" and "N" qualified variants gives customers flexibility to switch sourcing without re-qualification, since both variants share the same silicon die, mask set, and electrical specifications.

Best regards,

Peter

Tags (1)
No ratings
Version history
Last update:
a week ago
Updated by: