2409319_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2409319_en-US

2409319_en-US

S32ds 3.6.10 does not display example names.

No I2C/SPI routines for S32k14X could be found.

lixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.pnglixia_0-1787964602612.png

lixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.pnglixia_0-1787964995674.png


lixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.pnglixia_1-1787965022577.png

lixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.pnglixia_0-1787965109494.png


回复: S32ds3.6.10不显示example例称

See here


Their superiors have no idea what the shell is thinking.

Conclusion: You have to install a bunch of unnecessary software yourself.

If you need to open a colleague's old project or an old project you wrote yourself, it's safer to just use the current version + RTM; otherwise, you might run into problems.

Just soy sauce


Re: S32ds3.6.10不显示example例称

Hi@ lixia

S32K1 RTD 3.0.0QLP07 is not a complete RTD package; it simply adds support for some of the modules listed below.

Therefore, you cannot see the demo or select the RTD driver when creating a new project.

image.pngimage.pngimage.pngimage.pngimage.pngimage.pngimage.pngimage.pngimage.pngimage.pngimage.pngimage.png

You should first install S32K1 RTD 3.0.0.Install this package again.


@CY9 CY9

Your answer is incorrect; it pertains to RTD and RTM 4.0.2.They are completely different drivers, and the two should not be confused.

Re: S32ds3.6.10不显示example例称

You things:

After installing the new version of RTM, edited projects cannot be opened in the old RTM version.

You know the situation, right?


Therefore, it is not recommended to: [switch to a newer version], nor is it recommended to [use a different RTM version].

It's even suggested that you should never update the version and switch to a newer RTM!

That explanation makes sense!



Re: S32ds3.6.10不显示example例称

Don't you understand, " I think you created all these questions "?


Re: S32ds3.6.10不显示example例称

Hi@ CY9

The possible reason is that the RTM version pushed may be different for S32 DS installed at different times.

However, even if the pushed RTM version is different, you can still download different packages to choose to install different RTMs.

The rapid pace of version updates and the resulting compatibility issues have indeed caused confusion for users.

However, RTD and RTM 4.0.X are completely different drivers and should not be confused. S32 DS V3.4 is a very old version of IDE.

Re: S32ds3.6.10不显示example例称

Hi@ CY9

That's true. If you use different versions, you'll need to install multiple S32 DS versions, and only one RTD version can be installed under each S32 DS IDE.

Installing different RTDs on a single IDE is not allowed and will result in an error. However, with S32 DS, you can install multiple RTDs without conflict.

Re: S32ds3.6.10不显示example例称

This pot too: Re: [S32DS 3.5+RTM401] I don't know what this SHxT happened - NXP Community

Re: S32ds3.6.10不显示example例称

Hi@ CY9

I see that you created these problems. If the engineer in charge hasn't resolved your issue, you can continue to comment.

The responsible engineer will continue to follow up.



Re: S32ds3.6.10不显示example例称

Hi@ CY9

https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-5-RTM401-I-don-t-know-what-this-SHxT-happened...

https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-6-1-Update-Fail/m-p/2409828/emcs_t/S2h8ZW1haW...


What I mean is that you created these two posts, and each post has a dedicated engineer responsible for following up. If your problem hasn't been resolved, you can continue to comment.

Re: S32ds3.6.10不显示example例称

Ref : https://community.nxp.com/t5/S32-Design-Studio/S32DS-3-6-1-Update-Fail/mp/2409828/emcs_t/S2h8 ZW1haW...


It's already a complete mess!

Even NXP's own employees don't understand which RTM version is paired with which S32DS...


Version 3.5, which hasn't been updated at all, already provides RTM401. They even claim RTM401 is only compatible with version 3.3... ~_~'?


If you yourselves, who touch the same people every day, don't even understand it...

How can you expect someone who only uses their S32DS once every three to five months to understand it!?

It's a mess~ Completely messy.....



I never mentioned this concept. However, RTD and RTM 4.0.X are completely different drivers.

I'm just reminding you: Keep using whatever version and RTM you used in previous projects! Use it until you're dead!

Even if the new version of RTM/S32DS has some new/useful features... DO NOT update!!! It will kill you.

My daily work report is just: Install S32DS... How deep is Wu Yu's knowledge?


Re: S32ds3.6.10不显示example例称

Understood~

thank...

However, I don't think there will be a solution to these problems...


Because I have given up on v3.6.xAnd plans to remove v3.5 and reinstall v3.5+RTM.Go solve it~

And then... I'll never update again!




Re: S32ds3.6.10不显示example例称

Egg-like...


Colleague A uses v3.4+ without RTM

Colleague B uses v3.4+RTM401

Colleague C uses v3.4+RTM402

Colleague D is using v3.4 + RTM403

...

How would you like to work together with others?


Tags (1)
No ratings
Version history
Last update:
‎09-02-2026 04:33 AM
Updated by: