hi All,
Using : LX2160 LSDK 2108 main
MC firmware version: 10.32.0
DPDK Version : dpdk_19_11_tags_LSDK20.04-isc-09
Primary ( DPDK ) Process : Create a mbuff Pool using [ rte_pktmbuf_pool_create("dlmempool", ]
Secondary ( DPDK ) Process : fails to allocate mbuff using API [ rte_pktmbuf_alloc(mempool) ]
In Secondary i can see mempool is correct. I can see mbuff available is full. The failure happens for 1st mbuff allocation using rte_pktmbuf_alloc.
Any solution for this. Thanks.
Hello,
The secondary process must map hugepages at the same virtual address as the primary. If ASLR is active, the secondary will resolve the mempool pointer to a different virtual address, causing the first allocation to fail.
echo 0 > /proc/sys/kernel/randomize_va_space
Run this before launching either the primary or secondary process.
2. Provision Sufficient DPMCP Objects
Create as many DPMCP objects as the total number of processes (primary + secondary). For 1 primary + 1 secondary, you need at least 2 DMPCPs:
export DPMCP_COUNT=3 # for 1 Primary + 2 Secondary (always provision +1 as buffer)
./dynamic_dpl.sh dpmac.X
Each process needs its own DPIO portals. The formula is:
(Total Processes) × (cores per process + 1 extra per process)
For example, 1 primary (2 cores) + 1 secondary (2 cores) = at minimum 9 DPIOs.
export DPIO_COUNT=20 # set generously
The secondary process must NOT re-initialize I/O devices (dpni, dpbp, dpcon, dpseci). Only dpio and dpmcp should be initialized by the secondary. Pass the correct blacklist flags:
# Secondary process example — blacklist all dpni/dpbp/dpcon, allow only dpio + dpmcp
./your_secondary_app --proc-type=secondary \
-b fslmc:dpni.X \
-b fslmc:dpbp.X \
-b fslmc:dpcon.X \
-- [app args]
Or alternatively, explicitly whitelist only the dpio and dpmcp objects assigned to the secondary:
./your_secondary_app --proc-type=secondary \
-w fslmc:dpio.Y \
-w fslmc:dpmcp.Z \
-- [app args]
--proc-type=secondary EAL ArgumentEnsure the secondary is launched with the correct EAL flag:
./your_secondary_app -c -n 1 --proc-type=secondary ...
Or use --proc-type=auto to let DPDK auto-detect.
In the secondary, do not call rte_pktmbuf_pool_create again. Instead, look up the existing pool created by the primary:
// In secondary process:
struct rte_mempool *mempool = rte_mempool_lookup("dlmempool");
if (mempool == NULL) {
// Error: pool not found — ASLR or hugepage mapping issue
}
struct rte_mbuf *m = rte_pktmbuf_alloc(mempool);
If rte_mempool_lookup returns a valid non-NULL pointer but rte_pktmbuf_alloc still returns NULL, the issue is almost certainly the DPIO portal not being initialized for the secondary's thread/core.
Regards
thanks @Bio_TICFSL for the quick solution