2408520_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2408520_en-US

2408520_en-US

SafeRTOS Support and Package Availability for FRDM-A-S32K344

Hi NXP Team,

I am working with the FRDM-A-S32K344 development board based on the S32K344 MCU.

I would like to evaluate and integrate SafeRTOS for this platform. I have the following questions:

  1. Does NXP provide an officially supported SafeRTOS package or BSP/port for the FRDM-A-S32K344 / S32K344?
  2. Is there any SafeRTOS example or demo project available for S32K344?
  3. If NXP does not provide the SafeRTOS package directly, is there any recommended approach or partner from whom the SafeRTOS package can be obtained?
  4. Which SafeRTOS Cortex-M7 port layer and compiler configuration are recommended for the S32K344?
  5. Are there any reference projects, application notes, or integration guidelines available for integrating SafeRTOS with S32 Design Studio?

Currently, I am using FRDM-A-S32K344 and S32 Design Studio.

Any guidance regarding the supported SafeRTOS package, licensing, example projects, or integration procedure would be highly appreciated.

Thanks and regards.

Re: SafeRTOS Support and Package Availability for FRDM-A-S32K344

Hello,

1. Does NXP provide an officially supported SafeRTOS package or BSP/port for the FRDM-A-S32K344 / S32K344?

NXP does not develop or distribute the SafeRTOS package directly. SafeRTOS is a proprietary, safety-certified RTOS owned and licensed exclusively by WITTENSTEIN high integrity systems Ltd. (WHIS).

2. Is there any SafeRTOS example or demo project available for S32K344?

FreeRTOS examples such as:

FreeRTOS_Toggle_Led_Example_S32K344
Additional FreeRTOS-based reference applications for S32K3 platforms

These are included in the S32K3 FreeRTOS package.

3. If NXP does not provide the SafeRTOS package directly, is there any recommended approach or partner from whom the SafeRTOS package can be obtained?

SafeRTOS is developed and licensed by WITTENSTEIN high integrity systems (WHIS), not by NXP. According to WHIS documentation:

  • SAFERTOS is available for NXP S32K1 and S32K3 families.
  • WHIS provides processor/compiler-specific ports.
  • A Design Assurance Pack (DAP) and demonstration projects are available as part of the commercial package.
  • WHIS engineers port SAFERTOS to the specific S32K configuration requested by the customer.

4. Which SafeRTOS Cortex-M7 port layer and compiler configuration are recommended for the S32K344?

Since SafeRTOS is delivered by WHIS as a processor/compiler-specific package, the exact port depends on your selected toolchain.

The S32K344 uses an Arm Cortex-M7 core. WHIS states that SAFERTOS is delivered tailored to a specific processor/compiler combination rather than as a generic source package.

If you are using S32 Design Studio, you would typically discuss with WHIS which compiler variant you intend to use, for example:

GCC (S32DS default)
Green Hills
IAR

WHIS can then provide the appropriate certified port.

The S32K344 features a lockstep Arm® Cortex®-M7 core. Based on the available demo package and community guidance, the recommended configuration is:

Parameter

Recommended Value

SafeRTOS port layer

ARMv7M_MPU (Cortex-M7 with MPU support)

Compiler

ARM GCC 11.4 (NXP Embedded GCC for Arm v7)

Package identifier

009-006-252-003-246-002 WEB - ARMv7M_MPU GCC S32K344

The ARMv7M_MPU port is the correct choice because it leverages the Cortex-M7's Memory Protection Unit (MPU) — a mandatory requirement for SafeRTOS's memory isolation and ISO 26262 / ASIL compliance guarantees.

5. Are there any reference projects, application notes, or integration guidelines available for integrating SafeRTOS with S32 Design Studio?

The SafeRTOS_S32K344_Demo_Web readme (provided by WHIS inside the demo package) specifies the following verified toolchain:

Component

Version

S32 Design Studio IDE

v3.6.4

ARM GCC Compiler

11.4

S32K3 Real-Time Drivers (RTD)

6.0.0


Step-by-Step S32DS Setup:

  1. Open S32DS and go to Help → S32 Extensions and Updates. Install the latest versions of:

    • GNU ARM PEmicro Interface Debugging Support

    • GDB Client for Arm Embedded Processors

    • S32 Design Studio Platform package

    • S32K3xx development package

  2. Download S32K3 Real-Time Drivers (RTD) 6.0.0 from nxp.com:

    • Run the .exe installer

    • Add the remaining .zip update-site files via Help → S32 Extensions and Updates → Add sites

  3. Import the SafeRTOS S32K344 demo project provided by WHIS into S32DS.

  4. Install the WHIS Eclipse STATEVIEWER Plug-in — this is required for the demo to function correctly. The installation guide is included in the WHIS package as:

     34-185-AN-001-i3.0-Installing and Using the Eclipse STATEVIEWER Plug-in.pdf

    STATEVIEWER provides real-time task state visualization within the Eclipse/S32DS IDE for SafeRTOS debugging.

Best regards,

Peter


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎08-27-2026 02:33 AM
更新者: