大家好,论坛!
我尝试下载 LF-6.6.52_2.2.x 版本 imx-image-full 所需的软件包,但在下载 OpenCV extra 包时遇到了问题:要么耗时过长,要么下载失败。
khang at GL72-6QF in /devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp
$ bitbake imx-image-full --runall=fetch
Loading cache: 100% |#######################################################################################################################################################################| Time: 0:00:02
Loaded 5730 entries from dependency cache.
Parsing recipes: 100% |#####################################################################################################################################################################| Time: 0:00:00
Parsing of 3654 .bb files complete (3653 cached, 1 parsed). 5731 targets, 377 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mpevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky
meta-oe
meta-multimedia
meta-python
meta-freescale
meta-freescale-3rdparty
meta-freescale-distro
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x
meta-nxp-demo-experience
meta-nxp-matter-baseline
meta-nxp-openthread
meta-arm
meta-arm-toolchain
meta-clang
meta-gnome
meta-networking
meta-filesystems
meta-qt6
meta-parsec
meta-tpm
meta-virtualization = ":"
Sstate summary: Wanted 0 Local 0 Mirrors 0 Missed 0 Current 887 (0% match, 100% complete)################################################################################## | ETA: 0:00:00
Initialising tasks: 100% |##################################################################################################################################################################| Time: 0:00:05
NOTE: Executing Tasks
Setscene tasks: 887 of 887
Setscene tasks: 887 of 887
WARNING: opencv-4.10.0.imx-r0 do_fetch: Failed to fetch URL git://github.com/opencv/opencv_extra.git;destsuffix=extra;name=extra;branch=4.x;protocol=https, attempting MIRRORS if available
ERROR: opencv-4.10.0.imx-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/sysroots-uninative/x86_64-linux/usr/bin:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot-native/usr/bin/python3-native:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/sources/poky/scripts:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot/usr/bin/crossscripts:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot-native/usr/sbin:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot-native/usr/bin:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot-native/sbin:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/recipe-sysroot-native/bin:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/sources/poky/bitbake/bin:/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/hosttools"; export HOME="/home/khang"; LANG=C git -c gc.autoDetach=false -c core.pager=cat -c safe.bareRepository=all clone --bare --mirror https://github.com/opencv/opencv_extra.git /home/khang/Workspace/Ref/Platforms/NXP/iMX/NXP/yocto_dl/v6.6/git2/github.com.opencv.opencv_extra.git --progress failed with exit code 128, see logfile for output
ERROR: opencv-4.10.0.imx-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/opencv/opencv_extra.git;destsuffix=extra;name=extra;branch=4.x;protocol=https')
ERROR: Logfile of failure stored in: /devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/build-xwayland-8mp/tmp/work/armv8a-mx8mp-poky-linux/opencv/4.10.0.imx/temp/log.do_fetch.91350
ERROR: Task (/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/sources/meta-imx/meta-imx-bsp/recipes-support/opencv/opencv_4.10.0.imx.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1774 tasks of which 1773 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/devel/NXP/SW/imx-yocto-bsp-6_6_52-2_2_2/sources/meta-imx/meta-imx-bsp/recipes-support/opencv/opencv_4.10.0.imx.bb:do_fetch
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code. 请大家多多支持!
谢谢,并致以最诚挚的问候!
Khang
我这边进行了验证,运行以下命令后,大约花了 1 个小时才完成 git 源代码下载。
$ bitbake opencv -c patch -f
您可以尝试以下变通方法。
请进入 downloads/git2 文件夹执行以下操作:
嗨@yipingwang ,
看起来像是网络/位置问题。我尝试通过 VPN 连接,完全成功了。
顺祝商祺!
K.