Hi everyone, I was trying to run a SD-yocto image from the EMMC of a Bytesatwork Devboard ver 1.0 with an IMX93 chipset and managed to brick it when I changed the U-Boot variables in order to force it to boot from EMMC The image was the official Yocto Image (ver. 5.0.15) for the byteDevkit.
Since UART-Input doesn't get accepted anymore by the board no matter if I try to make console-inputs before, during or after turning on the board I can't do anything when trying to boot from SD-card.
Trying to flash an image directly into the EMMC via uuu and a USB-Connection hasn't been successful either. uuu recognizes the USB-connection with the command -lsusb but I always get an error saying pipeline -9 broke when trying to flash an image. I already changed the driver with zadig to WinUSB and use USB 3.0 since my laptop doesn't have USB 2.0-Ports.
Since I'm neither skilled nor knowledgeable enough to try and build a tweaked image to fix the problem if possible I'm honestly at my wits end and hope some of you may be able to help.
The System got bricked after I made the following change to the boot environment:
=> setenv bootcmd 'mmc dev 0; ext4load mmc 0:1 ${kernel_addr_r} /boot/Image; ext4load mmc 0:1 ${fdt_addr_r} /boot/imx93-bytedevkit.dtb; booti ${kernel_addr_r} - ${fdt_addr_r}'
=> saveenv
If I try to boot the System from the EMMC (Bootmode 0100) I get the following Output before the System freezes:
U-Boot SPL 2024.04-lf_v2024.04_6.6.52_2.2.x-r2+g82d4220bc6b+p0 (Jul 11 2025 - 05:04:16 +0000)
SOC: 0xa1009300
LC: 0x2040010
PMIC: PCA9451A
PMIC: Over Drive Voltage Mode
DDR: 3733MTS
M33 prepare ok
Normal Boot Trying to boot from BOOTROM
Boot Stage: Primary boot image offset 0x8000, pagesize 0x200, ivt offset 0x0
Load image from 0x58000 by ROM_API
NOTICE: TRDC init done
NOTICE: BL31: v2.10.0 (release):lf-6.6.52-2.2.1
NOTICE: BL31: Built : 06:40:36, Jul 7 2025
If I try to boot from an SD-card (Bootmode 1100) I get this Output before it freezes:
U-Boot 2024.04-lf_v2024.04_6.6.52_2.2.x-r2+g82d4220bc6b+p0 (Jul 11 2025 - 05:04:16 +0000)
Reset Status: POR
CPU: NXP i.MX93(52) Rev1.1 A55 at 1700 MHz
CPU: Industrial temperature grade (-40C to 105C) at 39C
Model: i.MX93 on bytesatwork byteDEVKIT
DRAM: 992 MiB
Core: 203 devices, 29 uclasses, devicetree: separate
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
Fail to setup video link
In: serial
Out: serial
Err: serial
BuildInfo:
- ELE firmware version 2.0.2-c4131933
UID: 401ce440f1124110bd234b09e4709d88
flash target is MMC:0
Net:
Warning: ethernet@428a0000 (eth1) using random MAC address - 9e:a6:f6:dc:09:91
Warning: ethernet@42890000 (eth0) using random MAC address - ce:8f:b2:02:6b:f5
eth0: ethernet@42890000, eth1: ethernet@428a0000 [PRIME]
Fastboot: Normal
Normal Boot
Autoboot in 1 seconds
switch to partitions #0, OK
mmc0(part 0) is current device
35777024 bytes read in 109 ms (313 MiB/s)
42568 bytes read in 2 ms (20.3 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Working FDT set to 83000000
Loading Device Tree to 000000008fff2000, end 000000008ffff647 ... OK
Working FDT set to 8fff2000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]
[ 0.000000] Linux version 6.6.52-r2-g472e64a0fc2c (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.4.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Tue Jul 8 12:00:06 UTC 2025
[ 0.000000] KASLR disabled due to lack of seed
[ 0.000000] Machine model: bytesatwork byteDEVKIT OSM i.MX93
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: 0x0000000096000000..0x0000000097dfffff (30720 KiB) nomap non-reusable optee_core@96000000
[ 0.000000] OF: reserved mem: 0x0000000097e00000..0x0000000097ffffff (2048 KiB) nomap non-reusable optee_shm@97e00000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4120000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node ele-reserved@a4120000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4120000..0x00000000a421ffff (1024 KiB) nomap non-reusable ele-reserved@a4120000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbfddb6c0-0xbfdddfff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x0000000095ffffff]
[ 0.000000] node 0: [mem 0x0000000098000000-0x00000000a411ffff]
[ 0.000000] node 0: [mem 0x00000000a4120000-0x00000000a421ffff]
[ 0.000000] node 0: [mem 0x00000000a4220000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges
[ 0.000000] cma: Reserved 32 MiB at 0x00000000bcc00000 on node -1
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: Embedded 22 pages/cpu s50856 r8192 d31064 u90112
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Virtualization Host Extensions
[ 0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line:
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 249856
[ 0.000000] Policy zone: DMA
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000b8c00000-0x00000000bcc00000] (64MB)
[ 0.000000] Memory: 859732K/1015808K available (21248K kernel code, 1658K rwdata, 7848K rodata, 4032K init, 641K bss, 123308K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[ 0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[ 0.000309] Console: colour dummy device 80x25
[ 0.000317] printk: console [tty0] enabled
[ 0.000688] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
[ 0.000706] pid_max: default: 32768 minimum: 301
[ 0.000759] LSM: initializing lsm=capability,integrity
[ 0.000843] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.000859] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[ 0.001572] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 0.002201] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.002289] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.002458] rcu: Hierarchical SRCU implementation.
[ 0.002468] rcu: Max phase no-delay instances is 1000.
[ 0.003234] EFI services will not be available.
[ 0.003397] smp: Bringing up secondary CPUs ...
[ 0.003815] Detected VIPT I-cache on CPU1
[ 0.003871] GICv3: CPU1: found redistributor 100 region 0:0x0000000048060000
[ 0.003907] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
[ 0.004022] smp: Brought up 1 node, 2 CPUs
[ 0.004033] SMP: Total of 2 processors activated.
[ 0.004041] CPU features: detected: 32-bit EL0 Support
[ 0.004048] CPU features: detected: 32-bit EL1 Support
[ 0.004056] CPU features: detected: Data cache clean to the PoU not required for I/D coherence
[ 0.004066] CPU features: detected: Common not Private translations
[ 0.004073] CPU features: detected: CRC32 instructions
[ 0.004083] CPU features: detected: RCpc load-acquire (LDAPR)
[ 0.004090] CPU features: detected: LSE atomic instructions
[ 0.004098] CPU features: detected: Privileged Access Never
[ 0.004104] CPU features: detected: RAS Extension Support
[ 0.004114] CPU features: detected: Speculative Store Bypassing Safe (SSBS)
[ 0.004176] CPU: All CPU(s) started at EL2
[ 0.004185] alternatives: applying system-wide alternatives
[ 0.008278] devtmpfs: initialized
[ 0.012419] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.012459] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.013204] pinctrl core: initialized pinctrl subsystem
[ 0.014406] DMI not present or invalid.
[ 0.014867] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.016071] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[ 0.016510] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.016929] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.017406] thermal_sys: Registered thermal governor 'step_wise'
[ 0.017414] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.017465] cpuidle: using governor menu
[ 0.017560] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.017622] ASID allocator initialised with 65536 entries
[ 0.018232] Serial: AMBA PL011 UART driver
[ 0.018290] imx mu driver is registered.
[ 0.018309] imx rpmsg driver is registered.
[ 0.023068] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver
[ 0.028173] platform 4ae10000.dsi: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/panel@0
[ 0.028214] platform 4ae10000.dsi: Fixed dependency cycle(s) with /soc@0/lcd-controller@4ae30000
[ 0.028435] platform 4ae10000.dsi: Fixed dependency cycle(s) with /soc@0/lcd-controller@4ae30000
[ 0.028493] platform 4ae30000.lcd-controller: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000
[ 0.030703] Modules: 23856 pages in range for non-PLT usage
[ 0.030713] Modules: 515376 pages in range for PLT usage
[ 0.031348] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.031378] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.031387] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.031394] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.031402] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.031410] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.031418] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.031425] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.032968] ACPI: Interpreter disabled.
[ 0.033767] iommu: Default domain type: Translated
[ 0.033793] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.034028] SCSI subsystem initialized
[ 0.034330] usbcore: registered new interface driver usbfs
[ 0.034361] usbcore: registered new interface driver hub
[ 0.034386] usbcore: registered new device driver usb
[ 0.035004] mc: Linux media interface: v0.10
[ 0.035046] videodev: Linux video capture interface: v2.00
[ 0.035092] pps_core: LinuxPPS API ver. 1 registered
[ 0.035101] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [email protected]
[ 0.035116] PTP clock support registered
[ 0.035269] EDAC MC: Ver: 3.0.0
[ 0.035732] scmi_core: SCMI protocol bus registered
[ 0.036098] FPGA manager framework
[ 0.036218] Advanced Linux Sound Architecture Driver Initialized.
[ 0.036772] Bluetooth: Core ver 2.22
[ 0.036809] NET: Registered PF_BLUETOOTH protocol family
[ 0.036817] Bluetooth: HCI device and connection manager initialized
[ 0.036829] Bluetooth: HCI socket layer initialized
[ 0.036838] Bluetooth: L2CAP socket layer initialized
[ 0.036856] Bluetooth: SCO socket layer initialized
[ 0.037251] vgaarb: loaded
[ 0.037658] clocksource: Switched to clocksource arch_sys_counter
[ 0.037857] VFS: Disk quotas dquot_6.6.0
[ 0.037885] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.038012] pnp: PnP ACPI: disabled
[ 0.043050] NET: Registered PF_INET protocol family
[ 0.043208] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.044113] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.044150] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.044165] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.044211] TCP bind hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.044493] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.044609] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.044643] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.044762] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.045174] RPC: Registered named UNIX socket transport module.
[ 0.045191] RPC: Registered udp transport module.
[ 0.045198] RPC: Registered tcp transport module.
[ 0.045204] RPC: Registered tcp-with-tls transport module.
[ 0.045211] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.046048] PCI: CLS 0 bytes, default 64
[ 0.046345] kvm [1]: IPA Size Limit: 40 bits
[ 0.046372] kvm [1]: GICv3: no GICV resource entry
[ 0.046381] kvm [1]: disabling GICv2 emulation
[ 0.046401] kvm [1]: GIC system register CPU interface enabled
[ 0.046427] kvm [1]: vgic interrupt IRQ9
[ 0.046455] kvm [1]: VHE mode initialized successfully
[ 0.047296] Initialise system trusted keyrings
[ 0.047511] workingset: timestamp_bits=42 max_order=18 bucket_order=0
[ 0.047754] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.048006] NFS: Registering the id_resolver key type
[ 0.048039] Key type id_resolver registered
[ 0.048047] Key type id_legacy registered
[ 0.048067] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.048077] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.048099] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.048292] 9p: Installing v9fs 9p2000 file system support
[ 0.069734] jitterentropy: Initialization failed with host not compliant with requirements: 9
[ 0.069757] Key type asymmetric registered
[ 0.069765] Asymmetric key parser 'x509' registered
[ 0.069818] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.069831] io scheduler mq-deadline registered
[ 0.069839] io scheduler kyber registered
[ 0.069876] io scheduler bfq registered
[ 0.073826] EINJ: ACPI disabled.
[ 0.078241] Bus freq driver module loaded
[ 0.085775] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.088108] 44380000.serial: ttyLP0 at MMIO 0x44380010 (irq = 17, base_baud = 1500000) is a FSL_LPUART
[ 0.088147] fsl-lpuart 44380000.serial: Serial: Console lpuart rounded baud ratefrom 187500 to 115200
[ 0.088267] printk: console [ttyLP0] enabled
[ 1.279060] imx-lcdif: probe of 4ae30000.lcd-controller failed with error -2
[ 1.287354] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with 4ae30000.lcd-controller
[ 1.301356] loop: module loaded
[ 1.305755] megasas: 07.725.01.00-rc1
[ 1.314046] tun: Universal TUN/TAP device driver, 1.6
[ 1.319701] thunder_xcv, ver 1.0
[ 1.322988] thunder_bgx, ver 1.0
[ 1.326238] nicpf, ver 1.0
[ 1.330111] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.337346] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.342694] hclge is initializing
[ 1.346035] e1000: Intel(R) PRO/1000 Network Driver
[ 1.350911] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.356668] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.361632] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.367561] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.372966] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.378547] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.384806] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.390842] sky2: driver version 1.30
[ 1.394867] usbcore: registered new interface driver catc
[ 1.400300] usbcore: registered new interface driver kaweth
[ 1.405868] pegasus: Pegasus/Pegasus II USB Ethernet driver
[ 1.411457] usbcore: registered new interface driver pegasus
[ 1.417131] usbcore: registered new interface driver rtl8150
[ 1.422796] usbcore: registered new device driver r8152-cfgselector
[ 1.429079] usbcore: registered new interface driver r8152
[ 1.434586] usbcore: registered new interface driver lan78xx
[ 1.440254] usbcore: registered new interface driver asix
[ 1.445666] usbcore: registered new interface driver ax88179_178a
[ 1.451774] usbcore: registered new interface driver cdc_ether
[ 1.457612] usbcore: registered new interface driver cdc_eem
[ 1.463281] usbcore: registered new interface driver dm9601
[ 1.468861] usbcore: registered new interface driver sr9700
[ 1.474443] usbcore: registered new interface driver CoreChips
[ 1.480289] usbcore: registered new interface driver smsc75xx
[ 1.486048] usbcore: registered new interface driver smsc95xx
[ 1.491802] usbcore: registered new interface driver gl620a
[ 1.497387] usbcore: registered new interface driver net1080
[ 1.503065] usbcore: registered new interface driver plusb
[ 1.508567] usbcore: registered new interface driver rndis_host
[ 1.514501] usbcore: registered new interface driver MOSCHIP usb-ethernet driver
[ 1.521906] usbcore: registered new interface driver cdc_ncm
[ 1.527579] usbcore: registered new interface driver huawei_cdc_ncm
[ 1.533859] usbcore: registered new interface driver cdc_mbim
[ 1.539618] usbcore: registered new interface driver r8153_ecm
[ 1.545875] VFIO - User Level meta-driver version: 0.3
[ 1.552654] usbcore: registered new interface driver cdc_wdm
[ 1.558531] usbcore: registered new interface driver uas
[ 1.563873] usbcore: registered new interface driver usb-storage
[ 1.569962] usbcore: registered new interface driver usbserial_generic
[ 1.576505] usbserial: USB Serial support registered for generic
[ 1.582517] usbcore: registered new interface driver ftdi_sio
[ 1.588268] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.595589] usbcore: registered new interface driver usb_serial_simple
[ 1.602118] usbserial: USB Serial support registered for carelink
[ 1.608224] usbserial: USB Serial support registered for flashloader
[ 1.614591] usbserial: USB Serial support registered for funsoft
[ 1.620604] usbserial: USB Serial support registered for google
[ 1.626532] usbserial: USB Serial support registered for hp4x
[ 1.632286] usbserial: USB Serial support registered for kaufmann
[ 1.638387] usbserial: USB Serial support registered for libtransistor
[ 1.644926] usbserial: USB Serial support registered for moto_modem
[ 1.651197] usbserial: USB Serial support registered for motorola_tetra
[ 1.657818] usbserial: USB Serial support registered for nokia
[ 1.663659] usbserial: USB Serial support registered for novatel_gps
[ 1.670021] usbserial: USB Serial support registered for siemens_mpi
[ 1.676390] usbserial: USB Serial support registered for suunto
[ 1.682320] usbserial: USB Serial support registered for vivopay
[ 1.688333] usbserial: USB Serial support registered for zio
[ 1.694007] usbcore: registered new interface driver usb_ehset_test
[ 1.701353] imx_usb 4c200000.usb: No over current polarity defined
[ 1.708038] UDC core: g_serial: couldn't find an available UDC
[ 1.715325] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0
[ 1.730471] bbnsm_rtc 44440000.bbnsm:rtc: registered as rtc0
[ 1.736808] bbnsm_rtc 44440000.bbnsm:rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.746038] i2c_dev: i2c /dev entries driver
[ 1.753139] imx7ulp-wdt 42490000.watchdog: imx93 wdt probe
[ 1.787402] Bluetooth: HCI UART driver ver 2.3
[ 1.791883] Bluetooth: HCI UART protocol H4 registered
[ 1.797022] Bluetooth: HCI UART protocol BCSP registered
[ 1.802352] Bluetooth: HCI UART protocol LL registered
[ 1.807488] Bluetooth: HCI UART protocol ATH3K registered
[ 1.812890] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.819284] Bluetooth: HCI UART protocol Broadcom registered
[ 1.824994] Bluetooth: HCI UART protocol QCA registered
[ 1.831298] sdhci: Secure Digital Host Controller Interface driver
[ 1.837532] sdhci: Copyright(c) Pierre Ossman
[ 1.842202] Synopsys Designware Multimedia Card Interface Driver
[ 1.848543] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.855334] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.863232] fsl-se secure-enclave: assigned reserved memory node ele-reserved@a4120000
[ 1.873387] fsl-se secure-enclave: Successfully registered ele-trng
[ 1.879142] random: crng init done
[ 1.879689] fsl-se secure-enclave: i.MX secure-enclave: hsm0 interface to firmware, configured.
[ 1.891850] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.898604] usbcore: registered new interface driver usbhid
[ 1.904183] usbhid: USB HID core driver
[ 1.904309] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA
[ 1.945753] imx93-adc 44530000.adc: ADC calibration failed!
[ 1.951368] imx93-adc: probe of 44530000.adc failed with error -11
[ 1.958480] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available
[ 1.968425] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.976335] optee: probing for conduit method.
[ 1.977451] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 1.980811] optee: revision 4.4 (ecea75b7fee5a3c8)
[ 1.987571] optee: dynamic shared memory is enabled
[ 1.987831] mmcblk0: mmc0:0001 016G01 14.5 GiB
[ 1.992772] optee: initialized driver
[ 1.998748] mmcblk0: p1
[ 2.004322] NET: Registered PF_LLC protocol family
[ 2.005920] mmcblk0boot0: mmc0:0001 016G01 8.00 MiB
[ 2.008032] u32 classifier
[ 2.013839] mmcblk0boot1: mmc0:0001 016G01 8.00 MiB
[ 2.017621] input device check on
[ 2.021299] mmcblk0rpmb: mmc0:0001 016G01 4.00 MiB, chardev (234:0)
[ 2.025176] Actions configured
[ 2.039098] NET: Registered PF_INET6 protocol family
[ 2.044802] Segment Routing with IPv6
[ 2.048507] In-situ OAM (IOAM) with IPv6
[ 2.052513] NET: Registered PF_PACKET protocol family
[ 2.057586] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 2.070641] Bluetooth: RFCOMM TTY layer initialized
[ 2.075541] Bluetooth: RFCOMM socket layer initialized
[ 2.080716] Bluetooth: RFCOMM ver 1.11
[ 2.084473] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.089778] Bluetooth: BNEP filters: protocol multicast
[ 2.094999] Bluetooth: BNEP socket layer initialized
[ 2.099961] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.105875] Bluetooth: HIDP socket layer initialized
[ 2.111098] 8021q: 802.1Q VLAN Support v1.8
[ 2.115320] lib80211: common routines for IEEE802.11 drivers
[ 2.121028] 9pnet: Installing 9P2000 support
[ 2.125419] Key type dns_resolver registered
[ 2.143506] registered taskstats version 1
[ 2.147939] Loading compiled-in X.509 certificates
[ 2.172921] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[ 2.181294] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[ 2.198616] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with ldb-phy
[ 2.210799] dw-mipi-dsi-imx 4ae10000.dsi: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/panel@0
[ 2.220052] mipi-dsi 4ae10000.dsi.0: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000
[ 2.228927] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.236979] imx-drm display-subsystem: bound 4ae10000.dsi (ops dw_mipi_dsi_imx_ops)
[ 2.244908] imx-drm display-subsystem: bound ldb-display-controller (ops imx93_ldb_ops)
[ 2.253294] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[ 2.802984] Console: switching to colour frame buffer device 60x53
[ 2.828150] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device
[ 2.837814] pps pps0: new PPS source ptp0
[ 2.846512] fec 42890000.ethernet eth0: registered PHC device 0
[ 2.853413] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[ 2.859635] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 2.866514] imx-dwmac 428a0000.ethernet: DWMAC4/5
[ 2.871338] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[ 2.878525] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[ 2.885704] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[ 2.892440] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[ 2.898623] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 2.906332] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 2.913173] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 2.920027] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 2.927635] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[ 2.942363] imx_usb 4c200000.usb: No over current polarity defined
[ 2.954776] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 2.961299] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 2.985668] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 2.993524] hub 1-0:1.0: USB hub found
[ 2.998921] hub 1-0:1.0: 1 port detected
[ 3.008793] Goodix-TS 0-005d: supply AVDD28 not found, using dummy regulator
[ 3.019083] Goodix-TS 0-005d: supply VDDIO not found, using dummy regulator
[ 3.125704] Goodix-TS 0-005d: Error reading 1 bytes from 0x8140: -5
[ 3.161700] Goodix-TS 0-005d: Error reading 1 bytes from 0x8140: -5
[ 3.197663] Goodix-TS 0-005d: I2C communication failure: -5
[ 3.206490] Goodix-TS: probe of 0-005d failed with error -5
[ 3.215233] i2c i2c-0: LPI2C adapter registered
[ 3.222451] nxp-pca9450 1-0025: No IRQ configured?
[ 3.224819] tca6418 1-0034: Device initialized
[ 3.227276] nxp-pca9450: probe of 1-0025 failed with error -22
[ 3.244047] Goodix-TS 1-005d: supply AVDD28 not found, using dummy regulator
[ 3.254216] Goodix-TS 1-005d: supply VDDIO not found, using dummy regulator
[ 3.361719] Goodix-TS 1-005d: Error reading 1 bytes from 0x8140: -5
[ 3.397698] Goodix-TS 1-005d: Error reading 1 bytes from 0x8140: -5
[ 3.433661] Goodix-TS 1-005d: I2C communication failure: -5
[ 3.442457] Goodix-TS: probe of 1-005d failed with error -5
[ 3.451205] i2c i2c-1: LPI2C adapter registered
[ 3.458342] imx_usb 4c100000.usb: No over current polarity defined
[ 3.471095] g_serial gadget.0: Gadget Serial v2.4
[ 3.477393] g_serial gadget.0: g_serial ready
[ 3.485854] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO
[ 3.486159] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.504424] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.513610] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 3.521940] mmc1: SDHCI controller on 42860000.mmc [42860000.mmc] using ADMA
[ 3.523888] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 3.531273] clk: Disabling unused clocks
[ 3.539449] cfg80211: failed to load regulatory.db
[ 3.557817] ALSA device list:
[ 3.562298] No soundcards found.
[ 3.568049] /dev/root: Can't open blockdev
[ 3.573684] VFS: Cannot open root device "" or unknown-block(0,0): error -6
[ 3.583559] Please append a correct "root=" boot option; here are the available partitions:
[ 3.594850] b300 15187968 mmcblk0
[ 3.594855] driver: mmcblk
[ 3.604564] b301 7497318 mmcblk0p1 076c4a2a-01
[ 3.604569]
[ 3.612052] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.612806] b320 8192 mmcblk0boot0
[ 3.625056] (driver?)
[ 3.634669] b340 8192 mmcblk0boot1
[ 3.634673] (driver?)
[ 3.644238] List of all bdev filesystems:
[ 3.644587] mmc1: new ultra high speed SDR104 SDXC card at address 0001
[ 3.648243] ext3
[ 3.648245] ext4
[ 3.648246] ext2
[ 3.648248] squashfs
[ 3.655362] mmcblk1: mmc1:0001 SD64G 58.3 GiB
[ 3.656759] vfat
[ 3.656761]
[ 3.656766] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 3.656770] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 6.6.52-r2-g472e64a0fc2c #1
[ 3.656775] Hardware name: bytesatwork byteDEVKIT OSM i.MX93 (DT)
[ 3.656778] Call trace:
[ 3.656780] dump_backtrace+0x90/0xe8
[ 3.656794] show_stack+0x18/0x24
[ 3.656801] dump_stack_lvl+0x48/0x60
[ 3.656807] dump_stack+0x18/0x24
[ 3.656811] panic+0x324/0x380
[ 3.656818] mount_root_generic+0x260/0x330
[ 3.656825] mount_root+0x170/0x334
[ 3.656829] prepare_namespace+0x6c/0x2a4
[ 3.656833] kernel_init_freeable+0x244/0x284
[ 3.656837] kernel_init+0x24/0x1dc
[ 3.656843] ret_from_fork+0x10/0x20
[ 3.656849] SMP: stopping secondary CPUs
[ 3.658689] Kernel Offset: disabled
[ 3.658690] CPU features: 0x0,c0000000,40028143,1000721b
[ 3.658694] Memory Limit: none
[ 3.789243] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---
Hello @Johny1
I hope you are doing very well.
As this is a third party Board and Software, we do not support it.
Please contact directly to Bytesatwork.
Best regards,
Salas.