Hello NXP,
I'm encountering incompatibility issues when using the following two RTDs. Could you please provide a solution? Thank you!
1. SW32K1_S32M24x_RTD_R21-11_3.0.0_QLP06_D2603_DesignStudio_updatesite
2. SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite
BramXiong_1-1787309606372.png
BramXiong_0-1787309530684.png
RTD_R23-11_7.0.1_D2603The Release Notes mention S32DS version 3.6.4. Is this the only version that can be used, or can S32DS still be used?3.6.10? Is the new version compatible with the old version?
BramXiong_0-1787309923367.pngBramXiong_0-1787309923367.png
Hi @BramXiong ,
I’m not from NXP, but I faced a similar issue before. The main problem in my case was related to the NXP-GCC version.
If you are facing the same issue with S32K 3.6, try changing the NXP-GCC version from 11.4 to 10.2. After doing this, the RTD platform should become visible.
I’ve attached an image for reference.
Hope this helps.
Regards,
Ganesh