Board: Z248 A0 EVB, blank MRAM (first-time flashing)
Probe: S32 Debug Probe — OS 1.1.0 / Boot Loader 1.0.1 (confirmed latest)
Tools: S32DS 3.6.6 + S32K5 Development Package 3.6.6 EAR + Debugger Core 3.6.10
SWD chain IS detected:
device[0]: core_type=S32K5(376)
device[1]: core_type=DAPv5(232)
But ccs_config_chain fails (ccs_error=39):
"S32K5: Initialization sequence is not found" (subcore error 73)
"S32K5: Bus error" (subcore error 76)
Verified OK: VTREF=3.3V, SRST_B=3.3V, J6/J9 in Debug Mode (Pin 3-4),
12V then 48V power sequence
Tried: LS and Non-LS M7 cores, JTAG 10MHz~2MHz, reset delay 0/500ms,
init scripts s32k5xx_attach.py / attach_first_instruction.py /
generic_bareboard.py / generic_bareboard_all_cores.py
Question:
Is initial boot-chain programming (HSE / IVT / DCD / Boot Manager / MICROSAR)
of a BLANK Z248 A0 supported via S32 Debug Probe + S32DS?
UM12524 section 4.7.1 documents the full flashing panel only for Lauterbach
TRACE32, while 4.7.2 assumes an already-built elf on a booting board.
If TRACE32 is mandatory for the first flashing, please confirm.
Hello @hjlim1 ,
I am writing to you in regard to a product currently in your possession – an NPI (New Product Introduction) which has not been officially launched yet.
Please be advised that customers who have been granted early access to such products have assigned their field engineers. Your designated field engineer should serve as your primary support channel for any issues, concerns or queries you may have about this product.
Our online support team will be opening a wider range of support for this product once it has been officially released. Until then, we will not be equipped to provide the desired assistance.
Thank you for your understanding.
Best regards,
Pavel