2406835_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2406835_en-US

2406835_en-US

PN7150: intermittent DISCOVERY_FAILED (0x60 07) and zeroed NDEF data with FeliCa Lite‑S (RC‑S966)

Hello, I am using the PN7150 reader IC and observing unstable behavior with FeliCa Lite‑S (RC‑S966) tags.

Even when the tag is placed directly on the antenna, I see repeating cycles of:

  • Correct UID frames

  • Correct NDEF frames

  • Zeroed NDEF frames

  • Empty NDEF frames

  • 0x60 07 (DISCOVERY_FAILED) notifications

Example CAN log:

  • UID (C040041): 01 2E 54 F7 C3 59 42 3E (always stable)

  • NDEF (C060041): Sometimes correct: D1 01 09 54 02 65 6E 48 / 65 6C 6C 6F 21 Sometimes zeroed: 00 00 00 00 00 00 00 00 / 00 00 00 00 00 Sometimes empty (DLC=0)

When the tag is slightly farther away (still within normal NFC range), PN7150 frequently reports 0x60 07 and restarts discovery.


My questions are

  1. Is it expected that PN7150 reports 0x60 07 when Lite‑S temporarily disables Polling or when RF field is slightly weak?

  2. Can Polling Disable cause PN7150 to return zeroed or empty NDEF data?

  3. Is there a recommended way to handle Lite‑S Polling Disable behavior in PN7150 firmware?

    • e.g., skip presence check, delay discovery restart, retry strategy

  4. Are there any PN7150 application notes specifically addressing FeliCa Lite‑S behavior?

A glance over canAnalyzer3 Mini is like this:

"No";"Time (abs)";"State";"ID (hex)";"DLC";"Data (hex)";"ASCII"
"3.261";"34505.380";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.262";"34505.381";" E ";" C040041";"2";"00 F1";".."
"3.263";"34506.401";" E ";" C060041";"0";"";""
"3.264";"34506.645";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.265";"34506.646";" E ";" C040041";"2";"00 F1";".."
"3.266";"34506.894";" E ";" C060041";"0";"";""
"3.267";"34507.143";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.268";"34507.143";" E ";" C040041";"2";"00 F1";".."
"3.269";"34507.389";" E ";" C060041";"0";"";""
"3.270";"34507.930";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.271";"34507.931";" E ";" C040041";"2";"00 F1";".."
"3.272";"34508.979";" E ";" C060041";"8";"00 00 00 00 00 00 00 00";"........"
"3.273";"34508.980";" E ";" C060041";"5";"00 00 00 00 00";"....."
"3.274";"34509.222";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.275";"34509.222";" E ";" C040041";"2";"00 F1";".."
"3.276";"34509.467";" E ";" C060041";"8";"00 00 00 00 00 00 00 00";"........"
"3.277";"34509.468";" E ";" C060041";"5";"00 00 00 00 00";"....."
"3.278";"34509.713";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.279";"34509.714";" E ";" C040041";"2";"00 F1";".."
"3.280";"34509.959";" E ";" C060041";"8";"00 00 00 00 00 00 00 00";"........"
"3.281";"34509.960";" E ";" C060041";"5";"00 00 00 00 00";"....."
"3.282";"34510.495";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.283";"34510.496";" E ";" C040041";"2";"00 F1";".."
"3.284";"34511.516";" E ";" C060041";"0";"";""
"3.285";"34511.759";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.286";"34511.760";" E ";" C040041";"2";"00 F1";".."
"3.287";"34512.005";" E ";" C060041";"0";"";""
"3.288";"34512.251";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.289";"34512.252";" E ";" C040041";"2";"00 F1";".."
"3.290";"34512.497";" E ";" C060041";"0";"";""
"3.291";"34512.739";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.292";"34512.739";" E ";" C040041";"2";"00 F1";".."
"3.293";"34512.985";" E ";" C060041";"8";"D1 01 09 54 02 65 6E 48";"...T.enH"
"3.294";"34512.986";" E ";" C060041";"5";"65 6C 6C 6F 21";"ello!"
"3.295";"34513.231";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.296";"34513.232";" E ";" C040041";"2";"00 F1";".."
"3.297";"34513.477";" E ";" C060041";"8";"D1 01 09 54 02 65 6E 48";"...T.enH"
"3.298";"34513.478";" E ";" C060041";"5";"65 6C 6C 6F 21";"ello!"
"3.299";"34513.724";" E ";" C040041";"8";"01 2E 54 F7 C3 59 42 3E";"..T..YB>"
"3.300";"34513.724";" E ";" C040041";"2";"00 F1";".."


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎08-21-2026 02:37 AM
更新者: