2406767_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2406767_en-US

2406767_en-US

S32K3 Standby RAM data modified before Reset_Handler

Hello,

When I debug S32K344 with PE Micro, I found that an array(__attribute__ ((section(".standby_data"))) volatile uint32_t WkupSourcestatus1[64];) located in the standby RAM section  is unexpectedly modified when entering main(). Then, as shown in the attached video, I manually modified the registers to reinitialize the standby RAM area. The data was correctly initialized to 0, and after entering main(), everything ran fine. However, after a reset, when I enter the Reset_Handler, the data in the WkupSourcestatus1 array is modified again. Why is this happening? I noticed that a large number of 0x5AA55AA5 values appear in the array. Is this related to the SBAF_BOOT_MARKER? I tested this on another board and the phenomenon is the same.

8.png8.png8.png8.png8.png8.png

Then I switched to using J-Link for debugging and found that no abnormality occurs during a reset while debugging. However, after a debug session is restarted, all data in the standby RAM area becomes 0xDEADBEEF. Is this expected behavior?

S32K344

S32DS3.6.4

RTD700

PE v.6.0.8


BR,

Jason

Re: S32K3 Standby RAM data modified before Reset_Handler

Hi

Sorry for the late reply; I've had a lot of inquiries to handle lately.

I suggest you refer to the discussion on S32K311 standby RAM retention for how to use standby RAM.

Best Regards,
Robin

Re: S32K3 Standby RAM data modified before Reset_Handler

The standby RAM content will remain during reset and the value you observed should be the content before MCU reset

=======================================================================================

The RAM is integrated by the SRAM memory and the TCM. Part of the SRAM memory is available in standby
mode. This means that the content of this memory are retained after setting the MCU in standby mode. The
S32K3 product family leverages the TCM feature of ARM Cortex M7 architecture, whose main purpose is to
provide a deterministic access time to the cores to some important data avoiding any delay in the access. This
feature can be exploited in Real Time Operating Systems.

As noted, the data stored in the Standby SRAM memory sourced by Standby domain is retained when
the MCU is in standby mode and available after the wakeup. But the data in SRAM sourced by Run
domain is not available and it needs to be initialized after the wakeup to avoid ECC errors. Is important
to remark that after wakeup, the Standby SRAM doesn't need to be initialized to avoid ECC error, but
the rest of the SRAM does need it, so a proper distinction should be performed in the Startup code. An
example to make this distinction is depicted in the following code.

Re: S32K3 Standby RAM data modified before Reset_HandlerHi

Sorry for the late reply.

In my test, I did not perform any sleep/wake-up operation. I only performed a reset through S32DS, and this caused the data in the standby RAM area to change. Checking the map file, the variable is indeed located in standby RAM (0x20400000). I checked the link you provided, and it seems to be unrelated to the issue in that link.

BR,
Jason
Tags (1)
No ratings
Version history
Last update:
yesterday
Updated by: