2406717_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2406717_en-US

2406717_en-US

iMX RT1052 multiple SDRAM

Hello,

I'm trying to wrap my head around how to use multiple SDRAM chips on the iMX1052.

In particular, I'm finding some inconsitencies between what's mentioned in the reference manual VS what's actually configurable on the MCUXpresso Config Tool Peripherals section.

From the manual, we have a total of 6 available pins for CS:

CS0, CSX0, CSX1, CSX2, CSX3, RDY

From the Peripheral section, when I enable SEMC in the Peripheral Drivers, I should be able to configure the multiple SDRAM banks, but when I go to select CS Pin Mux I only see:

CSX0, CSX1, CSX2, CSX3, RDY

I would expect to see CS0 in the list, and if selected I would also expect the Chip Selection menu to be greyed out (forced to SEMC SDRAM CS0).

Also, another inconsistency is that from this Peripheral section I can select one of the pins and configure Chip Selection menu to SEMC SDRAM CS0, which according to the Reference Manual table 29.7.1.3.3 CSXn/RDY pins cannot be set to CS0, they can only be set to CS1-2-3.

In any case, can you please explain how should I go about with configuring up to 4 SDRAM chips?

I would like to use CS0 for IC0, CSX1 on GPIO_SD_B1_07 for IC1, CSX2 on GPIO_SD_B1_08 for IC2, and RDY on GPIO_EMC_28 for IC3.

Kind regards,

Michele Perla

i.MXRT 105xi.MXRT 106xRe: iMX RT1052 multiple SDRAM

Hi Gavin, 

thanks for your reply. I still don't quite understand how I should configure the device using MCUXpresso Config Tool to use multiple SDRAM ICs.

SEMC_CS0 is hardwired to CS0; SEMC_CSX0 cannot be wired to CS0 output. So, why is there an option in the Config Tool to set CSX0 as CS0?

How can I properly configure the SDRAM with Config Tool to use SEMC_CS0 as CS0, RDY as CS1, SEMC_CSX0 as CS3, SEMC_CSX1 as CS3? I don't think I can.

I want to verify that all the pin mux is setup correctly for my purposes before I make my HW, but it's hard when the Tools and the Manual say different things.

Kind regards,

Michele

Re: iMX RT1052 multiple SDRAM

Hi @MichelePerla ,

Thanks for your interest in NXP MIMXRT series!

  1. SEMC_CS0 is a dedicated, fixed output for SDRAM CS0. The CS pin mux option is used only to configure the multiplexed CSX/RDY paths. Since SEMC_CS0 is not controlled by SEMC_IOCR.MUX_CSXn, it is not listed under CS pin mux.

  2. The RT1052 hardware does not support routing SDRAM CS0 through CSX0. Therefore, I believe this is an invalid option in the configuration tool. Please follow the Reference Manual definition.

  3. SEMC_RDY should be routed to GPIO_EMC_40.

Best regards,
Gavin

タグ(1)
評価なし
バージョン履歴
最終更新日:
木曜日
更新者: