2406529_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2406529_en-US

2406529_en-US

S32K312 LPSPI Slave mode

joshua9264_0-1787132569429.pngjoshua9264_0-1787132569429.pngjoshua9264_0-1787132569429.png

working:slave mode、4 lines

(B) is right or (C) is right?



Re: S32K312 LPSPI Slave mode

Hi @joshua9264 

Both configurations are valid.

By default, the LPSPI interface operates according to Option B, where:

  • SIN as the input data line, connected to the master's output.
  • SOUT as the output data line, connected to the master's input.

However, it is also possible to swap the data pin directions so that SOUT is used as the input data line and SIN is used as the output data line, which corresponds to Option C. To achieve this configuration, you need to set the CFGR1[PINCFG] field accordingly.


BR, VaneB

タグ(1)
評価なし
バージョン履歴
最終更新日:
昨日
更新者: