Dear NXP Community Team,
I am currently working with the NXP S32K1xx series board using the S32 Design Studio (S32DS) IDE.
I am looking for the S32SDK S32K1xx RTM 4.0.1 package for my development work. Could you please share the ZIP package or provide an official download link from where I can obtain this SDK version?
I specifically need S32SDK S32K1xx RTM 4.0.1 to ensure compatibility with my existing project and development environment.
I would appreciate your assistance.
Thank you.
Hi,
S32SDK S32K1xx RTM 4.0.1 was introduced in S32 Design Studio v3.4, you can refer to https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-S32-Platform-v3-...
The K1 packages can be installed on the product from the S32DS Extensions and Updates tool.
S32SDK S32K1xx RTM 4.0.1 can be added to S32DS 3.5 as well. So assuming that you have fresh S32DS v3.5 installation. First step is update existing packages:
Selecting the K1 dev package also install dependencies:
image (26).pngimage (26).png
Hope it helps.
BR, Petr