2405613_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2405613_en-US

2405613_en-US

USB ENUMERATION Issue with 2KL[IW610] MURATA MODULE

Hi NXP,


We have an issue with the IW610 DRIVER working with Ambarella processor-based SBC [Ambarella CV75 EVK]. The IW610 HW is the Murata 2KL Module which is connected to the host over USB interface. 

[DEVICE SETUP]: 

The setup is that the customer (VVDN) is using a 5G/LTE module + 2KL Module on the same host through a USB HUB -USB4216 from Microchip. 

[ISSUE]: At boot up the 2KL MODULE (IW610) is detected and enumerated correctly, but the 5G/LTE module detection is failing.  If the device is rebooted  with the 5G/LTE modules only connected to the system it enumerates correctly. 

The issue is seen whenever the other USB devices are getting enumerated post the enumeration of the 2KL module. All devices enumerated before the 2KL enumeration work correctly. 

Attached is the customer console logs and WiFi/BT driver Debug logs.

Looking forward to your support.

Thanks,

Pankaj Sant


Re: USB ENUMERATION Issue with 2KL[IW610] MURATA MODULE

Hello @pankaj 


Sure let me check your logs.


Best Regards

Shaun

Re: USB ENUMERATION Issue with 2KL[IW610] MURATA MODULE

Hi @shaun_wu ,


The issue is not related to external radio co existence but with the device enumeration over USB.


Can you support to investigate the enumeration issue with the provided logs. incase if you need additional logs kindly let us know.

Re: USB ENUMERATION Issue with 2KL[IW610] MURATA MODULE

Hello @pankaj 


For multiple radio chip, we provide external coexistence interface to control radio traffic. You may follow the guide to connect and configure coexistence: 

https://www.nxp.com/webapp/Download?colCode=AN14410&appType=license 


Best Regards

Shaun

Re: USB ENUMERATION Issue with 2KL[IW610] MURATA MODULE

Hello @pankaj 


We notice we have customer report same issue to us. And India SAE team is handling it. 00994762 | Case | Salesforce, you may do further discussion via this case. 


Best Regards

Shaun

Tags (1)
No ratings
Version history
Last update:
‎08-20-2026 04:28 AM
Updated by: