2405533_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2405533_en-US

2405533_en-US

Camera enablement (OV5647) for FRDM-IMX8MPLUS board

AN14376: https://docs.nxp.com/bundle/AN14376/page/topics/enable_omnivision_ov564

Wrt this post, I would like to enable camera on similar device FRDM-IMX8MPLUS Device.

I see, I am able to get some values and detection at 0x36 address which is OV5647.

I have tried to use .ko files or .binaries or .dtb of IMX8MPLUS EVK board.  Somehow, I am getting errors like repeating logs.


Booting from mmc ...

Failed to load 'imx8mp-evk-ov5647.dtb'

 

 

Total boot commands on changinf the .dtb file for ov5647 camera

 

Hit any key to stop autoboot:  0

Working FDT set to 43000000

libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND

libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND

libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND

libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND

libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND

libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND

starting USB...

Bus usb@38100000: Failed to initialize board for imx8m USB

probe failed, error -62

Bus usb@38200000: Register 2000140 NbrPorts 2

Starting the controller

USB XHCI 1.10

scanning bus usb@38200000 for devices... 1 USB Device(s) found

       scanning usb for storage devices... 0 Storage Device(s) found

 

Device 0: unknown device

MMC: no card present

switch to partitions #0, OK

mmc2(part 0) is current device

Scanning mmc 2:1...

MMC: no card present

Unable to open OP-TEE session (err=-5)

mm_communicate failed!

Error: Cannot initialize UEFI sub-system, r = 3

Running BSP bootcmd ...

switch to partitions #0, OK

mmc2(part 0) is current device

Failed to load 'boot.scr'

35633664 bytes read in 163 ms (208.5 MiB/s)

Booting from mmc ...

Failed to load 'imx8mp-evk-ov5647.dtb'

WARN: Cannot load the DT

u-boot=>

u-boot=> /boot/uEnv.txt

Unknown command '/boot/uEnv.txt' - try 'help'

 

Also, tell me how to remove previous saved environment as the device is stuck at same uboot even after rebooting...

WARN: Cannot load the DT 

 
My aim is to enable OV5647 on my FRDM-IMX8MPLUS board.

Any help is appreciated..






I2C detection output from com port logs:

root@imx8mpfrdm:~# i2cdetect -y 1

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:                         -- -- -- -- -- -- -- --

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

30: -- -- -- -- -- -- 36 -- -- -- -- -- -- -- -- --

40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

50: -- -- -- UU -- -- -- -- -- -- -- -- -- -- -- --

60: -- -- -- -- -- -- -- -- 68 -- -- -- -- -- -- --

70: -- -- -- -- -- -- -- --

root@imx8mpfrdm:~# i2cget -y 1 0x36 0x00

0x00

root@imx8mpfrdm:~# i2ctransfer -y 1 w2@0x36 0x30 0x0a r2

0x56 0x47 (intended as per sensor)





My gemini conversation link: https://share.gemini.google/WfVLaifz3gXB


Product FRDM-IMX8MPLUS Tagging randomly: @nxpenthusiast @nxp @techexplorer_139 
标记 (1)
无评分
版本历史
最后更新:
昨天
更新人: