2405165_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2405165_en-US

2405165_en-US

S32DS 3.6.2

I have a question about S32DS 3.6.2.I'm having an IDE configuration issue. I'm using a demo program generated by RTD 6.0.0, and I'm encountering the problem shown in the image below when configuring CT. What could be causing IVT and other tools to be disabled? I'm a bit confused. 屏幕截图 2026-08-14 155022.png

Re: S32DS 3.6.2

Hello @sunshine88 ,

IVT/DCD support in Configuration Tools depends on the selected device and on the scope implemented in the installed tool package. The fact that the IVT editor is disabled does not mean that the RTD example project is invalid.
 
For the selected S32K358 configuration, the graphical IVT/DCD editors are not available in Configuration Tools. These tools are related to BootROM/boot-image configuration and are not required for the standard projects.
 
Therefore, if Update Code and the project build complete successfully, the project can still be used normally for the supported configuration areas such as Pins, Clocks and Peripherals.

Best regards,

Pavel

Tags (1)
No ratings
Version history
Last update:
Saturday
Updated by: